During my installation Windows 7 32 bit, I was having problems with the installation. After several calls with Microsoft support we were able to resolve the issues. In a nut shell it was all about assembly version ( new DLL hell ! ). This is a summary that was sent to me from Microsoft. I may help to shed some light on this issue.
To briefly summarize:
You were encountering the following error dialog reporting a TypeLoadException on the following type:
{"Could not load type 'Microsoft.VisualStudio.Web.ToolboxItemConfiguration' from assembly 'Microsoft.VisualStudio.Web, Version=9.0.0.0, Culture=neutral, PublicKeyToken=b03f5f7f11d50a3a'.":"Microsoft.VisualStudio.Web.ToolboxItemConfiguration"}
This error occurred when the toolbox was attempting to refresh itself, after opening a winform in the winform designer. We investigated the scenario and found that the TypeLoadException was occurring due to an older (RTM version) of Microsoft.VisualStudio.Web.dll installed under the …\common7\ide directory. On a couple of other machine this error was not encountered.
Upon further investigation (using ildasm.exe) we found that the ToolboxItemConfiguration class is implemented in a more recent version of Microsoft.VisualStudio.Web.dll (from VS 2008 SP1), and installing VS 2008 SP1 on the problem system cleared up the problems.
You had an additional question related to the DeltaTau Powermac isolated shell installation. Specifically, after installing the DeltaTau software, you were encountering an error dialog “Cannot find one or more components. Please reinstall the application. To fix this, we had you download and install the VS 2008 Isolated Shell with SP1 redist, and this fixed up the problem with the DeltaTau software.