Jump to content
OMRON Forums

ACC-5E


Hersoft

Recommended Posts

Hi there,

 

I just got an ACC-5E and want to use it for a couple of things.

Mainly for the handwheel input and for the Display output.

 

When I put the board into my UMAC chassis and start UMAC configuration software I had expected to see an extra (unidentified maybe) I/O board or an Macro board.

I made sure there where no other boards in the chassis except for the Turbo Pmac and ofcourse the PSU.

 

Because I do not see any extra boards I think my ACC-5E is broken.

 

Is there any way to check it further?

 

Regards from Belgium, Otto.

 

Link to comment
Share on other sites

  • Replies 5
  • Created
  • Last Reply

Top Posters In This Topic

Hersoft,

 

Please make sure to issue a "$$$***" command. This will re-initialize the CPU, causing it to detect new hardware on the back plane. Once reinitialized, you can see the ACC-5E. The variable I4902 will show which address Gate2 has been detected on.

 

Regards,

Link to comment
Share on other sites

Hello Sina,

 

well I did just that and checked the value of I4902.

It came back wit $0 which can not be true i guess.

I put the card on the first address of the table and I got the Macro chip on it.

Any suggestions now?

 

regards, Otto.

Link to comment
Share on other sites

Hello Sina,

 

Here are the serial numbers.

 

ACC-5E (603447-101) S/N: C0007EQD

 

3U-Turbo (603766-104) S/N:C0003VNZ V1.942 5C0 (option)

 

I tried the ACC-5E also with a different CPU but this did not change the situation.

 

I hope this helps somewhat.

 

Regards, Otto.

Link to comment
Share on other sites

Hersoft,

 

Both your cards are new and they will not have any compatibility issue. If you have already tested the ACC-5E with another CPU and got the same result, it indicates a problem with ACC-5E. Please start an RMA process with Delta Tau customer support or through your Delta Tau distributor.

 

Regards,

Link to comment
Share on other sites

Guest
This topic is now closed to further replies.

×
×
  • Create New...