DTC-Kgu Posted October 11, 2011 Share Posted October 11, 2011 How do I know UMAC installed modbus? I can contol IO with ACC-65ETH home page but UMAC can't i67=$10700 M300->X:$10792,0,16 ; Discrete Outputs 1 – 16 (LSbit = Output 1) M301->Y:$10792,0,8 ; Discrete Outputs 17 - 24 M400->X:$10790,0,16 ; Discrete Inputs 1 – 16 (LSbit = Input 1) M401->Y:$10790,0,8 ; Discrete Inputs 17 - 24 modbus setup interface see attachment Link to comment Share on other sites More sharing options...
Sina.Sattari Posted October 11, 2011 Share Posted October 11, 2011 How do I know UMAC installed modbus? I can contol IO with ACC-65ETH home page but UMAC can't i67=$10700 M300->X:$10792,0,16 ; Discrete Outputs 1 – 16 (LSbit = Output 1) M301->Y:$10792,0,8 ; Discrete Outputs 17 - 24 M400->X:$10790,0,16 ; Discrete Inputs 1 – 16 (LSbit = Input 1) M401->Y:$10790,0,8 ; Discrete Inputs 17 - 24 modbus setup interface see attachment If you get connected to the device with Configure Ethernet 100 Base T software under Start > PMAC Executive PRO 2 > Delta Tau Common folder, you should see the Modbus option check marked. Also, if you don't have Modbus option, the Modbus setup page from PEWIN32PRO2 will notify you. You also have to make sure that you have defined at least 256 word in user buffer as your Modbus buffer memory. Link to comment Share on other sites More sharing options...
DTC-Kgu Posted October 28, 2011 Author Share Posted October 28, 2011 How do I know UMAC installed modbus? I can contol IO with ACC-65ETH home page but UMAC can't i67=$10700 M300->X:$10792,0,16 ; Discrete Outputs 1 – 16 (LSbit = Output 1) M301->Y:$10792,0,8 ; Discrete Outputs 17 - 24 M400->X:$10790,0,16 ; Discrete Inputs 1 – 16 (LSbit = Input 1) M401->Y:$10790,0,8 ; Discrete Inputs 17 - 24 modbus setup interface see attachment If you get connected to the device with Configure Ethernet 100 Base T software under Start > PMAC Executive PRO 2 > Delta Tau Common folder, you should see the Modbus option check marked. Also, if you don't have Modbus option, the Modbus setup page from PEWIN32PRO2 will notify you. You also have to make sure that you have defined at least 256 word in user buffer as your Modbus buffer memory. Hi Sina Thank you for answering ,I have solved the last question,Because the customer modified the gateway IP which could not communication. Now I have another problem,one ACC-65ETH can't communication with ETH and USB can't identify.I want to try to download firmware.Whether can send ACC-65ETH's firmware to me. regards Link to comment Share on other sites More sharing options...
Gregs Posted October 28, 2011 Share Posted October 28, 2011 I attached the com firmware for the ACC-65ETH and the PMAC; they should be used together. Downloading to the ACC-65 works the same as for PMAC. Also, you should have the latest PCOMM Server running. I also attached the boot strap firmware, just in case that is needed. Instructions for downloading com firmware are posted: http://forums.deltatau.com/showthread.php?tid=63&highlight=firmware Acc65ETH.zip Link to comment Share on other sites More sharing options...
DTC-Kgu Posted October 31, 2011 Author Share Posted October 31, 2011 Hi Gregs I have download the boot strap and ACC65ETH.iic to ACC65ETH, but USB can't be recongnized on the PC,and ETH can't communicate aslo. Link to comment Share on other sites More sharing options...
Recommended Posts