dzrong Posted April 9, 2012 Share Posted April 9, 2012 Hello Everyone, There is a Update in the V1.4 Firmware talking in the Power PMAC Software Reference Manual, it's "Fixed error trapping of invalid system commands by gpascii utility". What's problem will be cause by this error if using V1.3 Firmware? If new communication can't be established by GPASCII command,and tell you "Gpascii input/output error",is't possible cause by this error? Thanks Link to comment Share on other sites More sharing options...
Sina.Sattari Posted April 9, 2012 Share Posted April 9, 2012 dzrong, The problem which was fixed from 1.3 to 1.4 was caused by sending invalid system commands through "system" function. For example "system la" instead of a valid command "system ls". The problem you're mentioning usually is caused by a bad memory or bad connection between the flash memory daughter card and the CPU. Link to comment Share on other sites More sharing options...
Recommended Posts