dzrong
Members-
Posts
187 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Everything posted by dzrong
-
Is it possble to control “local” motors with ARM LS1021A CPU if the Acontis EtherCAT stack is used at the same time? If not ,what problems will happen? I had done some test, and it seemes that can work at an 1 kHz update rate.
-
I'm using ACC51E with PPmac,and find lots of niose in the ADC, I want to add a low pass filter to the ADC by EncTable,and get the Sinusoidal feedback position. But how to set that?
-
I want to control 3 axis X,Z and C move synchronously,is't possible to limit the velocity and acceleration of Axis C? For example: X10 Z20 C30
-
Why Synchronous M Variable not changed when program is running?
dzrong replied to dzrong's topic in Power PMAC
What is mean " non self referenced definition"? "M1->*" is what my M1 defined in my PPMAC. -
Hello EveryOne, I want to control 3 axis X,Z and C move synchronously,and I want to use the frax(x,z,c) to set the feedrate, but PPMAC seems not allow to do this,so how to control the speed of the three axis after some position points had been given? Thanks
-
Hello EveryOne, Why Synchronous M Variable not changed when program is running? The M1 always remain 0. Here is the program: N1G90M1==1 N2G1M1==2 N3F10M1==3 N4ta100M1==4 N5X30M1==5 N6Z0M1==6 N7F1M1==7 N8ta1M1==8 N9ts0M1==9 N10frax(x,z)M1==10 N11S1000M1==11 N12M3M1==12 N13X30Z0M1==13 N14X29.999Z0M1==14 N15X29.998Z0M1==15 N16X29.997Z0M1==16 N17X29.996Z0M1==17 N18X29.995Z0M1==18 N19X29.994Z0M1==19 N20X29.993Z0M1==20 N21X29.992Z0M1==21 N22X29.991Z0M1==22 N23X29.99Z0M1==23 N24X29.989Z0M1==24
-
Hello EveryOne, Why my C axis run so slow,only 20 block per second, The unit of C is degree. Coord[1].AltFeedRate=1000000 Motor[3].MaxSpeed=1000 Coord[1].PosRollover[2]=-360 Here is the program: &1#1->1000000X-30000000 &1#2->1000000Z-30000000 &1#3->C // open prog 4 // --------------------User Code Goes Here------------------------ linear abs ta 1 ts 0 tm 1 C 0.01 C 0.02 C 0.03 C 0.04 C 0.05 C 0.06 C 0.07 C 0.08 C 0.09 C 0.1 C 0.11 C 0.12 C 0.13 C 0.14 C 0.15 C 0.16 C 0.17 C 0.18 C 0.19 C 0.2 C 0.21 C 0.22 C 0.23 C 0.24 C 0.25 C 0.26 C 0.27 C 0.28 C 0.29 C 0.3 C 0.31 C 0.32 C 0.33 C 0.34 C 0.35 C 0.36 C 0.37 C 0.38 C 0.39 C 0.4 C 0.41 C 0.42 C 0.43 C 0.44 C 0.45 C 0.46 C 0.47 C 0.48 C 0.49 C 0.5 C 0.51 C 0.52 C 0.53 C 0.54 C 0.55 C 0.56 C 0.57 C 0.58 C 0.59 C 0.6 C 0.61 C 0.62 C 0.63 C 0.64 C 0.65 C 0.66 C 0.67 C 0.68 C 0.69 C 0.7 C 0.71 C 0.72 C 0.73 C 0.74 C 0.75 C 0.76 C 0.77 C 0.78 C 0.79 C 0.8 C 0.81 C 0.82 C 0.83 C 0.84 C 0.85 C 0.86 C 0.87 C 0.88 C 0.89 C 0.9 C 0.91 C 0.92 C 0.93 C 0.94 C 0.95 C 0.96 C 0.97 C 0.98 C 0.99 C 1 close
-
How to get the abs position from an Endat2.2 with incremental encoder?
dzrong replied to dzrong's topic in Power PMAC
Dear CharlesP, I only think,maybe which Master of Delta Tau had done that before as what I'm doing,so we can solved the problem more simple. That's all. -
Hello Everyone, I'm using ACC84E with PPmac,and want to get the abs position from an Endat2.2 with incremental encoder,The type of Linear grating is LIP211,0.03125nm per count(LSB).A 36($24)-bit encoder from HEIDENHAIN. Now the position can be read correctly throw Acc84E[1].Chan[0].SerialEncDataA and Acc84E[1].Chan[0].SerialEncDataB after some setting like: Acc84E[1].SerialEncCtrl=$002003; Acc84E[1].Chan[0].SerialEncCmd =$071424; But I can't get a valid data of the RM_bit ,it's always zero even I move the motor go throw the whole trip by hand. Of course proper command codes had been send before,like: Acc84E[1].Chan[0].SerialEncCmd = $381424 Acc84E[1].Chan[0].SerialEncCmd = $421424 Because RM_bit is one bit of Acc84E[1].Chan[0].SerialEncDataC.SerialEncDataC is always zero,so RM_bit should be zero. And the ACC84E very new,should be the latest firmware to support the function. Does Anyone had using the Encoder like me? Can you give some suggestion?
-
Do you mean I can change password by typing the new password in the "Password" space,and Connect directly,and then the new password will be auto changed?
-
Hello EveryOne, For protecting source code reason, I want to change password of PPmac,by default is "deltatau",who can give me a complete process step by step to change the password? Thanks
-
Hello everyone, I set i260=3, and I want to know which Extension Period is now by using a plc0. I think there is a count in TURBO PMAC which maybe 0\1\2\3, maybe it's a open memory and how can I get it? Thanks
-
Hello, I have a big program about 1000000 block in it,and I want to download it to the PPmac, but an error:out of memory happenned.If the program size very small,everything works well. My question is that,we know PPmac have very big memory about 1G,why 30M zise block cause a "Out of memory"? Thanks.
-
a motor to follow a user calculate value every servo cycle
dzrong replied to dzrong's topic in Power PMAC
How to access Motor[2].MasterPos in the user servo program of motor 1 ? Motor[2].MasterPos can't be used directly. -
a motor to follow a user calculate value every servo cycle
dzrong replied to dzrong's topic in Power PMAC
If the position was calcalated in the realtime routines ,is Data Structure of Mptr->MasterPos supported in the user_pid_ctrl(struct MotorData *Mptr) or user_phase(struct MotorData *Mptr)? -
Hello, For some reason,I want to motor to follow a position every servo cycle,the position was calculated by the foreground PLC.Usually I will set ECT to get data from a user address and make Ix05 point to the ECT in Turbo,so the moter will follow the value of the address.But how to do that in Power Pmac? Or there are some simple way to do that?
-
Hello, Is there any Acc-??? support RESOLVER of TURBO or Non-Turbo PMAC PCI card? It seem only 58E support that for UMAC.
-
Motor Data Reporting Buffer (Used if I48 = 1 or I57 = 1)
dzrong replied to dzrong's topic in Turbo PMAC
Hello CharlesP, I want to get position information of Clipper though DPRAM. When enabled DPRAM foreground function,PMAC will auto copy the motor information to DPRAM,including position and so on. After that,I want to get the Position information though DPRAM by PC,in the PC side Visual Studdio C# was be used. So,after "using PCOMMSERVERLib" in the C#, Pmac.DPRGetLong(m_nDevice, 156, out i_x, out dpsucess) can get the DPRAM memory data,'156' is the host PC Address 0x009C which is the Motor net actual position of Memory Map.Of course the host PC Address 0x00A0 also include part information of Motor net actual position. After I get both 0x009C and 0x00A0 data,the Motor net actual position will be calculated,but how to calculate? -
How to get position using Turbo DPRAM? I want to get position through DPRAM by the momery 0x009C of the motor 1, DP:$060xxx-$060xxx+1 Motor net actual position (1/[ixx08*32] cts) In the C#: Pmac.DPRGetLong(m_nDevice, 156, out i_x, out dpsucess); Pmac.DPRGetLong(m_nDevice, 160, out i_x_h, out dpsucess); I get position data in i_x and i_x_h, but how to get position by the i_x_h and i_x? Thanks
-
Hello Gregs, Where can i get the manual of ACC-24S3? Thanks
-
Hello KEJR, Thank you for so much more and more characters reply. I had found the reason:one character write wrong because me. I have a more knowledge of seral port of power Pmac because you reply.
-
Is it possble to support 8 axis of power clipper? Just like acc-1p with clipper.
-
Because the value was 8bits data,that will be same in my application if or not have the `double`.And I had got other values expect 0x13... So that will not the key of my problem.
-
The 0x13/ 0x11 /0x0D is the apecial character of Linux,0x13 is Enter,0x11 is ^Q,ix13 ^s. So must disable the system function of this characters. This may be done though setting options.c_lflag. But I can get it out. If you can help me to try that,you can send that character using serial port,and recieve it itself(only connect the serail port send pin and recieve pin),if 0x13/ 0x11 /0x0D can be sent and recieve correctly,we win! I change a little code of the examle, so the serial port can send Hex, thought P var,we can get the recieve value If p1001 can be 0x13, my problem is solved.
-
Manually Scheduling Threads in Power PMAC
dzrong replied to Omron Forums Support's topic in Power PMAC
Yes,you are right.If this file is closed in IDE,no error happenned.