sbrun Posted November 30, 2012 Share Posted November 30, 2012 When, after a link break, i try reconnect for "unsolicited" : the .StartUnsolicitedEvent() make an exception with the message : "Error: The following SendFiles are locked and being used, 0, 1, 2, 3, 4" I use PPcomLib v1.0.0.1 (PowerPmacComLib.dll dated 29/06/2012) PPmac firmware 1.5.8.0 In my application (or with demo "PowerPmacComLibVBDemoApp") : - All ways to communicate with PPmac (including Unsolicited) work ok - When i disconnect the Ethernet link, - Problems of connections are normaly detected and i close all communications - I connect again the ethernet link - I launch all the re-connections, - All is ok execept for "unsollicited" where an exception occurs on .StartUnsolicitedEvent() with the message : "Error: The following SendFiles are locked and being used, 0, 1, 2, 3, 4" Same test can be done simply with the IDE and a unsolicited box opened : - Disconnect the Ethernet link, - Restore the Ethernet and reconnect the IDE - In the Unsolicited box, the red message is displayed : "Unable to connect to SSH's Unsolicited thread with error Error: The following SendFiles are locked and being used, 1, 2, 3, 4" - The only way that i found to restore, is to send to PPmac a "$$$" Link to comment Share on other sites More sharing options...
Omron Forums Support Posted December 4, 2012 Share Posted December 4, 2012 When, after a link break, i try reconnect for "unsolicited" : the .StartUnsolicitedEvent() make an exception with the message : "Error: The following SendFiles are locked and being used, 0, 1, 2, 3, 4" I use PPcomLib v1.0.0.1 (PowerPmacComLib.dll dated 29/06/2012) PPmac firmware 1.5.8.0 In my application (or with demo "PowerPmacComLibVBDemoApp") : - All ways to communicate with PPmac (including Unsolicited) work ok - When i disconnect the Ethernet link, - Problems of connections are normaly detected and i close all communications - I connect again the ethernet link - I launch all the re-connections, - All is ok execept for "unsollicited" where an exception occurs on .StartUnsolicitedEvent() with the message : "Error: The following SendFiles are locked and being used, 0, 1, 2, 3, 4" Same test can be done simply with the IDE and a unsolicited box opened : - Disconnect the Ethernet link, - Restore the Ethernet and reconnect the IDE - In the Unsolicited box, the red message is displayed : "Unable to connect to SSH's Unsolicited thread with error Error: The following SendFiles are locked and being used, 1, 2, 3, 4" - The only way that i found to restore, is to send to PPmac a "$$$" We are checking the issue and update the forum! Atul Link to comment Share on other sites More sharing options...
Recommended Posts