JeffLowe Posted January 3, 2013 Posted January 3, 2013 Is a delay of 10-15 seconds from the point where gathering is started in the IDE to when data is actually starting to be acquired normal?
Sina.Sattari Posted January 3, 2013 Posted January 3, 2013 10 to 15 seconds seems excessive. There is a small delay which is related to download and setup of the gather parameters, but it should be around 1 seconds or less. However, depending on how much background time is available and how the CPU is being utilized by foreground tasks and also number of active communication channels this time may grow. Would you be able to share your Power PMAC CPU usage time and percentage information from the task manager in the IDE?
Recommended Posts