Bharat Posted March 9, 2013 Share Posted March 9, 2013 Master Motor Reading - Encoder - 10000 cts/rev Max Speed - 300 rpm Slave Motor Reading - Encoder - 10000 cts/rev Ball Screw Pitch - 10 mm/rev of motor I want to run the slave motor, which should starts at 0 degree of master & should stop slave 100 degree of the master. The changing parameter for running the machine are as follows, 1. Slave distance Range - 1 mm to 10 mm 2. Master Speed Range - 1 to 300 rpm Can some body hep me in these to achieve the result to calculate RTIF. I am working Turbo Clipper . Bharat Vinchwekar[/size] Link to comment Share on other sites More sharing options...
steve.milici Posted March 11, 2013 Share Posted March 11, 2013 Master Motor Reading - Encoder - 10000 cts/rev Max Speed - 300 rpm Slave Motor Reading - Encoder - 10000 cts/rev Ball Screw Pitch - 10 mm/rev of motor I want to run the slave motor, which should starts at 0 degree of master & should stop slave 100 degree of the master. The changing parameter for running the machine are as follows, 1. Slave distance Range - 1 mm to 10 mm 2. Master Speed Range - 1 to 300 rpm Can some body hep me in these to achieve the result to calculate RTIF. I am working Turbo Clipper . Bharat Vinchwekar[/size] I have attached an application note describing PMAC Timebase setup.timebase.pdf Link to comment Share on other sites More sharing options...
Recommended Posts