Jump to content
OMRON Forums

Using PPMAC EtherCAT Master without Axis Module


kjcho

Recommended Posts

Hi,

 

I'm using Power PMAC EtherCAT Master.

Is it possible to use EtherCAT Master without Axis Module?

 

I tried to use only power module & cpu module, but EtherCAT Master doesn't work...

 

Furthermore, I'm considering using only cpu module with external power supply. (even without rack)

 

How can I implement these system?

 

Thank you.

Teyun.

Link to comment
Share on other sites

  • Replies 1
  • Created
  • Last Reply

Top Posters In This Topic

Top Posters In This Topic

Yes.

 

Since you don't have hardware interrupts with an axis card you must use the cpu's built in timer interrupt. In this case the cpu, power supply and ethernet card are all that is required.

 

Therefore, Sys.ServoPeriod to the desired period usually 1000msec or 500msec and Sys.CPUTimerIntr=1 then save and power cycle.

 

You must order the EtherCAT option when ordering the CPU so that you get the EtherCAT compatible network card. I assume you have done this.

 

Also there is the Power PMAC Etherlite product

 

http://www.deltatau.com/DT_Products/ProductDetailDescription.aspx?CatID=P10-POWER%20PMAC%20ETHERLITE

 

 

Hi,

 

I'm using Power PMAC EtherCAT Master.

Is it possible to use EtherCAT Master without Axis Module?

 

I tried to use only power module & cpu module, but EtherCAT Master doesn't work...

 

Furthermore, I'm considering using only cpu module with external power supply. (even without rack)

 

How can I implement these system?

 

Thank you.

Teyun.

Link to comment
Share on other sites

Guest
This topic is now closed to further replies.

×
×
  • Create New...