kmonroe023 Posted October 1, 2013 Posted October 1, 2013 I think I found a bug with the System Setup Program in the IDE. After a factory default reset ($$$***), a system that contains Acc24E3 cards seems to default to a 4 channel setup, even if 2 channel cards are installed in the backplane instead. When the System Setup Program is used to setup motors on the 2 channel Gate3 cards, some of the "Addressing" elements don't seem to get set properly, leaving these elements at their default 4 channel equivalent. See the attached jpg file for a screenshot from the Setup Variables applet right after using System Setup on a motor. Most of the elements associated with commutation get setup correctly, but a few elements pertaining to flags don't get set, and can cause a little confusion when trying to home these motors. Currently running IDE ver 1.5.0.21. (If this isn't the correct place to report this, please let me know). Regards, kmonroe
Sina.Sattari Posted October 1, 2013 Posted October 1, 2013 We are still developing the system setup and it is not completed yet. The registers which are left untouched are mostly related to homing/capturing mechanism which hasn't been implemented yet. Hopefully we can get to complete these steps soon.
Recommended Posts