cdmize Posted January 15, 2014 Share Posted January 15, 2014 I know this is a long shot, but can an ACC-12B be used with the Turbo on the JDISP port? The ACC-12B is an 8 digit display that was used with the SMCC to display axis position. I'm replacing an old SMCC with at UMAC Turbo and the machine has an ACC-12B and the customer likes it because the characters are large and easy to read from a distance. I read in the SMCC manual that its display port also supported the ACC-12A which the Turbo supports also. Given this, I want to know if the ACC-12B can be used with the Turbo and if so what would be the software settings. Link to comment Share on other sites More sharing options...
steve.milici Posted January 16, 2014 Share Posted January 16, 2014 It is electrically compatible but I think the character count is smaller and may just scroll the screen continuously. Link to comment Share on other sites More sharing options...
Recommended Posts