rjiyi Posted January 31, 2014 Share Posted January 31, 2014 We have a old Delta Tau Turbo PMAC system, it includes Turbo PMAC CPU (3A0 603382) and ACC-54E Ethernet card(3R2 603467) and Axis analog interface cards. My PC is WinXP + SP3. The system was running before but stopped for few years, I am trying to reuse it now. It can be running with PLC software stand alone, I just want connect it to do some modification, but I get some trouble with Ethernet and USB comunication. For Ethernet: I can Ping the IP address of the Delta Tau which was setup before, the Ethernet connection looks fine. Then I launch PEWIN32PRO2, Setup, Insert the PMAC device with the IP address, then run Test, after long time waiting, popup a message “The PMAC could not be detected”, then I reping the IP in windows, it will fail. I have to reboot PC and Delta Tau to get the IP back, but PMAC still could not be detected. For USB: I can see USB device in Device Manager as "Delata Tau Ethernet Comm Board", I want to insert a new device in Pro2 Setup, but I can see only COM1 and Pmac ETH0 in Available PMAC Devices, there is no USB item. Can any one give me some help? I am fairly new for Delta Tau. Thanks. Link to comment Share on other sites More sharing options...
Omron Forums Support Posted February 4, 2014 Share Posted February 4, 2014 Try running PeWin32Pro2 as an administrator first. You should then be able to see the missing devices. Link to comment Share on other sites More sharing options...
Recommended Posts