Leo Posted May 16, 2014 Share Posted May 16, 2014 I have a camera link to the CLIPPER card through ETHERNET with MODBUS. I still want to use PEWIN32 communicate to the CLIPPER through the ETHERNET . Can I use a router as below[refer to the attachment]? Link to comment Share on other sites More sharing options...
Sina.Sattari Posted May 16, 2014 Share Posted May 16, 2014 Yes. However, please keep in mind that the Modbus and Ethernet communication to PC are using the same resources and this may limit the bandwidth for one side if the other process has high demand for bandwidth. Link to comment Share on other sites More sharing options...
Recommended Posts