RomanSolonto Posted September 3, 2014 Share Posted September 3, 2014 Good day. I'm trying to set up a laser CNC. Laser radiation power should depend on the current (actual) feedrate. I need to make some variable ActualFeedrate-depended. In PHMI Designer I can use GetVectorVelocity(0) to view the current feedrate. How can I get actual feedrate and use it to set ACC-59E DAC ch#1 (m4602->Y:$78E08,0,12,U)? Link to comment Share on other sites More sharing options...
Omron Forums Support Posted September 5, 2014 Share Posted September 5, 2014 Isx89 indicates the most recently issued feedrate command by means of the F or TM command. sx = 50 + (Coordinate system number), so for coordinate system 1, I5189. See page 189 of the Turbo SRM for more details. Link to comment Share on other sites More sharing options...
RomanSolonto Posted September 8, 2014 Author Share Posted September 8, 2014 Thank you. But I need to calculate instant vector feedrate (use only X- and Y- axis). If I cut a square - in each corner instant vector feedrate will be 0, then it will accelerate, but I5189 will keep value. How can I get feedrate in each corner? Link to comment Share on other sites More sharing options...
curtwilson Posted September 8, 2014 Share Posted September 8, 2014 Most people who do this assign M-variables to the instantaneous desired velocity registers for each axis, then take the vector sum. This works better than noisy instantaneous actual velocity values. For example, define: M160->X:$86,0,24,S ; Motor 1 instant cmd vel register M260->X:$106,0,24,S ; Motor 2 instant cmd vel register Then in a PLC program: P60=SQRT(M160*M160+M260*M260) ; Instantaneous vector velocity M4602=P60*P61 ; Scale and output Link to comment Share on other sites More sharing options...
RomanSolonto Posted September 9, 2014 Author Share Posted September 9, 2014 Thank you very match. Link to comment Share on other sites More sharing options...
cmcdonald Posted September 9, 2014 Share Posted September 9, 2014 Most people who do this assign M-variables to the instantaneous desired velocity registers for each axis, then take the vector sum. This works better than noisy instantaneous actual velocity values. For example, define: M160->X:$86,0,24,S ; Motor 1 instant cmd vel register M260->X:$106,0,24,S ; Motor 2 instant cmd vel register Then in a PLC program: P60=SQRT(M160*M160+M260*M260) ; Instantaneous vector velocity M4602=P60*P61 ; Scale and output I think M160 and M260 have to be multiplied by 3/(I108*32) to get into counts/mS Chris Link to comment Share on other sites More sharing options...
Recommended Posts