Jump to content
OMRON Forums

problem with ACC57EY in MACRO station


Leo
 Share

Recommended Posts

UMAC MASTER + Macro station with 16X MACRO CPU.

There are 3 ACC24E2A cards and 3 ACC57EY cards on Macro station. The same as the Master .

 

Information about Macro station.

3*ACC-24E2A with OPT1A, base address :

UMAC MASTER + Macro station with 16X MACRO CPU.

There are 3 ACC24E2A cards and 3 ACC57EY cards on Macro station. The same as the Master .

 

Information about Macro station.

3*ACC-24E2A with OPT1A, base address :

S1-1 S1-3 S1-4 Board No.

ON ON ON 1

OFF ON ON 2

ON OFF ON 3

 

3*ACC-57EY (Yaskawa absolute encoder)

$A800,$B800,$8840

 

The 3rd ACC-57EY on Macro station can’t work well .

A week ago,channel 1 and 2 can get the absolute position when power on but channel 3 and 4 can not .

Now, none of them can work well.The hardware is well because I had exchanged the 2nd with 3rd card.

The configuration of the Macro is in attachment. Is there anything wrong ?

MACRO configuration.txt

Link to comment
Share on other sites

  • Replies 0
  • Created
  • Last Reply

Top Posters In This Topic

Popular Days

Top Posters In This Topic

Guest
This topic is now closed to further replies.
 Share


×
×
  • Create New...