Jump to content
OMRON Forums

PMAC-PC 602191


unreal91
 Share

Recommended Posts

Hello, DT support.

I have the desire to build a simple 3-axes Mill Machine with spindle. I am writing to you for help.

I have set:

1. PMAC-PC 602191-104, 4 Axes

2. CPU board Option 2602705-557 (60Mhz)

3. DPRAM, 602240-101

I Have Windows XP

In PEWIN-32Pro I fixed the link to the card using IRQ5 (E83 on board), the ISA Bus Base Address Control I/O 021F-0210

(and jmp E66 and E71 's set-OFF), D4000-D7FFF. Motor setup-Ok! DPRAM Test-Ok!

I can not create a machine in the PMAC-NC Pro2 Runtime. When you create a project, the PEWIN finds errors in the PLC.

Tested, there are variables that are designed for other PMAC.

It is possible that PMAC-NC Pro2 Runtime (ver 5.2) is not designed for PMAC-602191 PC-104 or NC5X.phm file?

I really hope to help. Will send the necessary files.

Link to comment
Share on other sites

  • Replies 6
  • Created
  • Last Reply

Top Posters In This Topic

We no longer sell NC software for non-Turbo PMAC. Please keep in mind that the hardware you have is very old and obsolete. I would recommend upgrading your hardware to one of the Turbo PMAC products like the Turbo Clipper with the DPRAM option. This will be compatible with the PMAC-NC Pro2 Runtime software.
Link to comment
Share on other sites

Understand the business.

I'm building a Machine for the soul in my apartment. I like Deltatau, but money for such purchases not. Perhaps you have available in the archive NC software for my PMAC under Windos XP. Sorry for my English I live in Ukraina.

Link to comment
Share on other sites

Guest
This topic is now closed to further replies.
 Share


×
×
  • Create New...