seankim Posted May 11, 2015 Share Posted May 11, 2015 I'm tryinng to install ACC-8ES on Power Clipper. Please let me know setting parameter. Link to comment Share on other sites More sharing options...
steve.milici Posted May 11, 2015 Share Posted May 11, 2015 Use the System Setup of the IDE. It will automatically set up these accessories. Link to comment Share on other sites More sharing options...
Ernst.Q Posted November 21, 2016 Share Posted November 21, 2016 I am trying to set-up the 8ES accessory with the Power Clipper, but the IDE set-up does not work. I upgraded the Power clipper with the latest firmware (in 2 steps) and the latest IDE. For some reason the setup utility does not work, I get the following error messages. Can you give me the settings for the DACstrobe and DACshift? Outputs system ethercat -m0 xml //11/17/2016 :12:53 PM - 192.168.0.200 system ethercat master // 11/17/2016 :12:53 PM - 192.168.0.200 Sys.MaxEcats = 1 // 11/17/2016 :12:53 PM - 192.168.0.200 Error messages 11/17/2016 :12:53 PM - 192.168.0.200, Module - Setup Motor : Global mask: 0xffffffff 11/17/2016 :12:53 PM - 192.168.0.200, Module - Setup Motor : CS mask: 0x201ffc 11/17/2016 :12:53 PM - 192.168.0.200, Module - Setup Motor : Motor mask: 0xc01ffd 11/17/2016 :12:53 PM - 192.168.0.200, Module - Setup Motor : Macro ring mask: 0x1e 11/17/2016 :12:53 PM - 192.168.0.200, Module - Setup Motor : Update period: 1.000000 Sec 11/17/2016 :12:53 PM - 192.168.0.200, Module - Setup Motor : Sys.Default=1 @ 17-11-2016 12:53:13 Debug messages 11/17/2016 :12:53 PM - 192.168.0.200, Module - Setup Motor Container : There was some error while executing database query. Details : Database Error:Table 'ppmac192_168_0_200.hardware_tbl1' doesn't exist. 11/17/2016 :12:53 PM - 192.168.0.200, Module - Setup Motor : There are no EtherCAT devices connect to Master[0]. 11/17/2016 :12:53 PM - 192.168.0.200, Module - Setup Motor Container : There was some error while executing database query. Details : Database Error:Table 'ppmac192_168_0_200.hardware_tbl1' doesn't exist. 11/17/2016 :12:53 PM - 192.168.0.200, Module - Global Clock : Empty Servo hardware List Link to comment Share on other sites More sharing options...
Omron Forums Support Posted November 21, 2016 Share Posted November 21, 2016 Gate3[1].DacStrobe=$FFFFC000 or =$FFFFE000. Motor[x].DacShift=0. I will work on a configuration, but meanwhile, please email your configuration to Support@Deltatau.com. Link to comment Share on other sites More sharing options...
Ernst.Q Posted November 25, 2016 Share Posted November 25, 2016 Dacstrobe =$7fffc000 works. I already tried that value before, but it did not look correct since the command signal still changed after the out0 command, slowly climbing to 10V. Looking a bit further I noticed this was cause by the fact the current loop enabled by default! So the signal changed was probably caused by the offset on the analog input. After setting motor[].pAdc =0 everything worked fine. Link to comment Share on other sites More sharing options...
Recommended Posts