Leo Posted July 22, 2015 Share Posted July 22, 2015 I changed the password of root , but the new password get lost when reboot the PPMAC. How to save the new password? Since I have no idea about Linux, a few other questions need answer. How to install LINUX program through POWER IDE? Will it be saved in flash? Link to comment Share on other sites More sharing options...
shansen Posted July 22, 2015 Share Posted July 22, 2015 See this thread: http://forums.deltatau.com/showthread.php?tid=83 Here is the short version. Mount the filesystem as read-write by issuing: mount -o remount,rw / Then use passwd to change the root password. When you are finished, sync the filesystem and remount as read-only: cd /.readonly/etc-tmpfs-mirror/ cp -a * ../etc/ cd /.readonly/root-tmpfs-mirror/ cp -a * ../root/ cd /.readonly/var-tmpfs-mirror/ cp -a * ../var/ mount -o remount,ro / Link to comment Share on other sites More sharing options...
windell747 Posted July 23, 2015 Share Posted July 23, 2015 Thank you shansen. When I run your first "cp" step I get the following error. /# cp -a * ../etc/ cp: writing `../etc/bin/bzcat': No space left on device cp: writing `../etc/bin/gunzip': No space left on device cp: writing `../etc/bin/bzip2': No space left on device is there something that I am doing wrong? See this thread: http://forums.deltatau.com/showthread.php?tid=83 Here is the short version. Mount the filesystem as read-write by issuing: mount -o remount,rw / Then use passwd to change the root password. When you are finished, sync the filesystem and remount as read-only: cd /.readonly/etc-tmpfs-mirror/ cp -a * ../etc/ cd /.readonly/root-tmpfs-mirror/ cp -a * ../root/ cd /.readonly/var-tmpfs-mirror/ cp -a * ../var/ mount -o remount,ro / Link to comment Share on other sites More sharing options...
shansen Posted July 23, 2015 Share Posted July 23, 2015 Hmmm. Check the output of df -h to make sure you have free disk space. Also check df -i to make sure you haven't run out of inodes. If you have a logger writing a lot of small files you could potentially have free disk space but run out of inodes. At this point I would reboot the Power PMAC, change the password, and then sync the filesystem. Link to comment Share on other sites More sharing options...
shansen Posted July 23, 2015 Share Posted July 23, 2015 Also, why is it trying to copy bzcat, gunzip, etc? Are you sure that you ran the cd /.readonly/etc-tmpfs-mirror/ command to switch directories before the cp -a * ../etc? My /.readonly/etc-tmpfs-mirror folder has the following contents: root@etc-tmpfs-mirror: ls -l total 12 -rwxr-xr-x 1 root root 283 2011-03-16 08:24 hosts -rw-r--r-- 1 root root 678 2015-05-09 06:31 mtab drwxrwxrwx 3 root root 80 2011-03-16 08:24 network -rw-r----- 1 root shadow 728 2015-05-08 15:05 shadow drwxr-xr-x 3 root root 60 2009-10-08 11:52 udev -r--r--r-- 1 root root 0 1981-08-26 17:25 .wh..wh.aufs drwx------ 2 root root 40 1981-08-26 17:25 .wh..wh.orph drwx------ 2 root root 40 1981-08-26 17:25 .wh..wh.plnk root@etc-tmpfs-mirror: Link to comment Share on other sites More sharing options...
windell747 Posted July 25, 2015 Share Posted July 25, 2015 Thanks Shansen! I think I got it to work. I put an extra space by accident in between the "/" and the "." in that cd command. It seems that the password has stayed now. I just tried uploading new code however, and I'm getting the following error "Could not Connect to Power Pmac FTP client, ...." I think this is because I changed the password because it started only after I had changed the password. Any ideas? thanks, windell Also, why is it trying to copy bzcat, gunzip, etc? Are you sure that you ran the cd /.readonly/etc-tmpfs-mirror/ command to switch directories before the cp -a * ../etc? My /.readonly/etc-tmpfs-mirror folder has the following contents: root@etc-tmpfs-mirror: ls -l total 12 -rwxr-xr-x 1 root root 283 2011-03-16 08:24 hosts -rw-r--r-- 1 root root 678 2015-05-09 06:31 mtab drwxrwxrwx 3 root root 80 2011-03-16 08:24 network -rw-r----- 1 root shadow 728 2015-05-08 15:05 shadow drwxr-xr-x 3 root root 60 2009-10-08 11:52 udev -r--r--r-- 1 root root 0 1981-08-26 17:25 .wh..wh.aufs drwx------ 2 root root 40 1981-08-26 17:25 .wh..wh.orph drwx------ 2 root root 40 1981-08-26 17:25 .wh..wh.plnk root@etc-tmpfs-mirror: Link to comment Share on other sites More sharing options...
shansen Posted July 25, 2015 Share Posted July 25, 2015 This might be an IDE issue. We don't typically use the Delta Tau IDE, so I don't know if they let you specify a non-standard root password. I just tried connecting to the FTP on one of our Power PMACs by browsing to ftp://[iP ADDRESS] in Windows explorer and everything worked correctly. Link to comment Share on other sites More sharing options...
Recommended Posts