aaqqxx Posted July 27, 2015 Share Posted July 27, 2015 Now I use PowerBrickLV,and I want to use PLC and motion programs that I wrote for using in TurboPMAC2. I must modify some code in PLC and motion programs,because some parameters change the unit(for example IXX26),it cause error. So I want to know do you have tool to do this translate,or may you design one?If you use python to do this,can you share the code with us? Link to comment Share on other sites More sharing options...
curtwilson Posted July 27, 2015 Share Posted July 27, 2015 Our experience with conversion programs of the type you ask for, including ones from other vendors that we have tried to use ourselves, is that they do not actually help. They will never get 100% of the conversion correct, and you spend more time trying to find the few issues converted improperly than you would with a totally manual conversion. The Software Reference Manual contains a chapter showing the necessary conversion for all Turbo PMAC I-variables, including unit differences. There is also a chapter of similar conversions for Turbo PMAC suggested M-variables. Link to comment Share on other sites More sharing options...
Recommended Posts