macs Posted March 4, 2016 Share Posted March 4, 2016 Hi, When I was trying to build and download a project that contains only codes files that are generated by Simulink-Power PMAC Interface, the error messages appeared: C:\Users\admin\AppData\Local\Temp\alvvhkv0.u5w\Temp\PowerPmac7.ppproj(0,0): Error : make: *** /opt/powerpc-465-rootfs/usr/src/linux-3.2.21-serengeti-smp: No such file or directory. Stop. Actually I can build the same project without error messages at another computer which is not connected to a PPMAC. And I also tired to reinstall the PPMAC IDE, when I first ran it in 'No Device' Mode, I could successfully build it. But after I connected to the PPMAC, I can't build it again anymore, even in offline mode. Here are the error messages appeared when I build the same project in offline (No device) Mode: C:\Users\admin\AppData\Local\Temp\alvvhkv0.u5w\Temp\PowerPmac7.ppproj(0,0): Error : /usr/local/dtlibs/libppmac/libppmac.so: undefined reference to `__wrap_printf' C:\Users\admin\AppData\Local\Temp\alvvhkv0.u5w\Temp\PowerPmac7.ppproj(0,0): Error : /usr/local/dtlibs/libppmac/libppmac.so: undefined reference to `__wrap_fwrite' C:\Users\admin\AppData\Local\Temp\alvvhkv0.u5w\Temp\PowerPmac7.ppproj(0,0): Error : /usr/local/dtlibs/libppmac/libppmac.so: undefined reference to `__wrap_fprintf' C:\Users\admin\AppData\Local\Temp\alvvhkv0.u5w\Temp\PowerPmac7.ppproj(0,0): Error : /usr/local/dtlibs/libppmac/libppmac.so: undefined reference to `__wrap_puts' C:\Users\admin\AppData\Local\Temp\alvvhkv0.u5w\Temp\PowerPmac7.ppproj(0,0): Error : /usr/local/dtlibs/libppmac/libppmac.so: undefined reference to `__wrap_free' C:\Users\admin\AppData\Local\Temp\alvvhkv0.u5w\Temp\PowerPmac7.ppproj(0,0): Error : /usr/local/dtlibs/libppmac/libppmac.so: undefined reference to `__wrap_fputs' C:\Users\admin\AppData\Local\Temp\alvvhkv0.u5w\Temp\PowerPmac7.ppproj(0,0): Error : collect2: ld returned 1 exit status Could somebody help me, please? Link to comment Share on other sites More sharing options...
Recommended Posts