Jump to content
OMRON Forums

apt-get fails


Dan.Allard

Recommended Posts

I am trying to setup lighttpd on a power pmac. I have the power pmac connected to the web through a DNS server and I can ping www.google.com successfully from the pp. When I try to do an

apt-get update

or

apt-get build-dep lighttpd

I get a long list of error messages about not being able to resolve the mirror.anl.gov

sample error message.

Err http://mirror.anl.gov lenny/main libglib2.0-0 2.16.6-2

Could not resolve 'mirror.anl.gov'

 

I have tried pinging this server from my mac as well as the pp and I am unable to reach it from either machine.

 

I have the source code for lighttpd but when i try to run the configuration program it give me the following error

configure: error: pcre-config not found, install the pcre-devel package or build with --without-pcre

 

I am in the process of setting up lighttpd to host a cgi webpage programmed in C++ so I could probably compile without pcre as it is related to pearl but i would like to build it with pearl support.

Link to comment
Share on other sites

  • Replies 7
  • Created
  • Last Reply

Top Posters In This Topic

I think this forum link below is the same problem I am seeing. I don't know how I would go about changing the update source as it suggest in the link below or if it is a good idea.

http://forums.debian.net/viewtopic.php?f=30&t=78447

 

Here is the output from my apt-get update it looks to be the same issue discussed in the link above.

 

192.168.0.21:/opt/ppmac# apt-get update

Ign http://security.debian.org lenny/updates Release.gpg

Ign http://security.debian.org lenny/updates/main Translation-en_US

Ign http://security.debian.org lenny/updates Release

Ign http://security.debian.org lenny/updates/main Packages/DiffIndex

Ign http://security.debian.org lenny/updates/main Sources/DiffIndex

Err http://mirror.anl.gov lenny Release.gpg

Could not resolve 'mirror.anl.gov'

Err http://mirror.anl.gov lenny/main Translation-en_US

Could not resolve 'mirror.anl.gov'

Ign http://security.debian.org lenny/updates/main Packages

Ign http://security.debian.org lenny/updates/main Sources

Ign http://security.debian.org lenny/updates/main Packages

Ign http://security.debian.org lenny/updates/main Sources

Err http://security.debian.org lenny/updates/main Packages

404 Not Found [iP: 128.31.0.63 80]

Err http://security.debian.org lenny/updates/main Sources

404 Not Found [iP: 128.31.0.63 80]

Ign http://volatile.debian.org lenny/volatile Release.gpg

Ign http://volatile.debian.org lenny/volatile/main Translation-en_US

Ign http://volatile.debian.org lenny/volatile Release

Ign http://volatile.debian.org lenny/volatile/main Packages/DiffIndex

Ign http://volatile.debian.org lenny/volatile/main Sources/DiffIndex

Ign http://volatile.debian.org lenny/volatile/main Packages

Ign http://volatile.debian.org lenny/volatile/main Sources

Ign http://volatile.debian.org lenny/volatile/main Packages

Ign http://volatile.debian.org lenny/volatile/main Sources

Err http://volatile.debian.org lenny/volatile/main Packages

301 Moved Permanently [iP: 130.89.148.14 80]

Err http://volatile.debian.org lenny/volatile/main Sources

301 Moved Permanently [iP: 130.89.148.14 80]

Reading package lists... Done

W: Failed to fetch http://mirror.anl.gov/debian/dists/lenny/Release.gpg Could not resolve 'mirror.anl.gov'

 

W: Failed to fetch http://mirror.anl.gov/debian/dists/lenny/main/i18n/Translation-en_US.bz2 Could not resolve 'mirror.anl.gov'

 

W: Failed to fetch http://security.debian.org/dists/lenny/updates/main/binary-powerpc/Packages 404 Not Found [iP: 128.31.0.63 80]

 

W: Failed to fetch http://security.debian.org/dists/lenny/updates/main/source/Sources 404 Not Found [iP: 128.31.0.63 80]

 

W: Failed to fetch http://volatile.debian.org/debian-volatile/dists/lenny/volatile/main/binary-powerpc/Packages 301 Moved Permanently [iP: 130.89.148.14 80]

 

W: Failed to fetch http://volatile.debian.org/debian-volatile/dists/lenny/volatile/main/source/Sources 301 Moved Permanently [iP: 130.89.148.14 80]

 

W: Some index files failed to download, they have been ignored, or old ones used instead.

W: You may want to run apt-get update to correct these problems

root@192.168.0.200

Link to comment
Share on other sites

I am a little feather along now. When I made the change listed in the other thread I was able to get it to start an update but I ended up with an error need to add sources to source.list. I found a debian source list generator below but i don't know which version of debian is the correct one to build a source list for. My concern is that i don't want to have the update try to update the kernel by mistake.

https://debgen.simplylinux.ch/

Link to comment
Share on other sites

1.) Make your disk writable

 

mount -o remount,rw /

 

2.) Next you must update the repository list file. Debian lenny is used on a 460 CPU so you must change the repositories to archive.debian.org.

 

deb http://archive.debian.org/debian/ lenny main non-free contrib

deb-src http://archive.debian.org/debian/ lenny main non-free contrib

deb http://archive.debian.org/debian-security/ lenny/updates main non-free contrib

deb-src http://archive.debian.org/debian-security/ lenny/updates main non-free contrib

 

The sources.list file placed in /etc/apt should look like what is above

 

3.) next issue the apt-get update command to reload the repositories. You can disregard the KEYEXPIRED warning message that comes back

 

 

4.) next issue the apt-get install lighttpd command to install lighttpd

 

lighttpd is now installed.

 

5.) Make sure the modifications from the apt-get install command make it to the readonly etc folder. Do this by issuing the following command

 

cp -a /.readonly/etc-tmpfs-mirror/* /.readonly/etc/

 

6.) Put the disk back to readonly mode

mount -o remount,ro /

Link to comment
Share on other sites

Henry I have to change the port for lighttpd to port 81. There is a program mono listening on port 80. Any idea what mono is and why it would be listening on port 80? I ask because 80 is the default http port so it would be nice to put the web server on 80 but I don't know what mono is or why it would be on port 80.
Link to comment
Share on other sites

Guest
This topic is now closed to further replies.

×
×
  • Create New...