ScottB Posted May 13, 2016 Share Posted May 13, 2016 I am trying to use the Plot tool to display a simple XY plot with my X Motor Actual Position as the Horizontal axis and the Y Motor Actual Position as the Left Axis. Is there a way to force the scaling of the vertical axis to be the same as the horizontal axis? Without this, my arcs end up looking like ellipses. Link to comment Share on other sites More sharing options...
steve.milici Posted May 16, 2016 Share Posted May 16, 2016 You can “right-mouse” click in the plot window and select “Properties”. Under the “General” tab you can select the axis to scale. Then under the “Scale” tab you can enter the values you desire. Link to comment Share on other sites More sharing options...
Recommended Posts