sbrun Posted November 28, 2016 Share Posted November 28, 2016 We have two BrickController-LV linked over MACRO. One in MACRO Ring master, the other in Slave state. All is working (in Torque-mode) ok. On the Slave, in IDE, the view MACRO-Status has the bit "AuxSlaveConfigFault" set. What means this bit ? (nothing in documentations). What could be the cause of this information ? Thanks in advance. Link to comment Share on other sites More sharing options...
Gregs Posted November 29, 2016 Share Posted November 29, 2016 Make sure that the MacroEnableX nodes enabled on the Slave are also enabled on the Ring Master. The "AuxSlaveConfigFault" set means it observed another Slave on this node which is Bit 10 of the MacroFlags going across the ring. See if “CLRF” on the Master and or the Slave clears the problem. Link to comment Share on other sites More sharing options...
Recommended Posts