Jump to content
OMRON Forums

GEO MACRO Communication Reset


MattReid

Recommended Posts

Hi

I have a GeoMACRO Drive connected to a GEOBRICK as the MACRO Master. Everything was working fine and MACRO was setup and communicating. After using an MS4,MI996 to a value of $F4037 (It was $F4030 before when working) and saving and resetting, I cannot access it the drive through MACRO anymore.

Using the MACRO ASCII setup does not see the drive. Starting right from a $$$*** and using MACRO ASCII setup in PEWIN32PRO2 fails to see the drive. I have a 24M2A and a 65M which can be communicated with but the GEOMACRO drive will not. The green MACRO light is illuminated and no errors are present but no ASCII communication available.

1. Can I reset it to factory defaults some how?

2. Can I access the I variables on the drive using the USB port on the front? I can open the port but how is it supposed to work? Straight terminal commands (if so I got no response) or PEWIN32PRO2?

 

Thanks

Matt

Link to comment
Share on other sites

  • Replies 1
  • Created
  • Last Reply

Top Posters In This Topic

Top Posters In This Topic

Guest
This topic is now closed to further replies.

×
×
  • Create New...