Jump to content
OMRON Forums

build fail - SOLVED


cmg2496

Recommended Posts

Hi,

 

I am trying to build and download a project that I have had working (building and downloading fine) previously from a different computer.

 

I have copied the project files over to a new computer, and when I try to build and download from this computer, I get a build failure with the following output:

 

'Please wait while Executing Project Script.

Please wait while mapping Power PMAC variables.

End of syncing the database.

PMAC variables are mapped successfully.

Build Process For usralgo.ko has started.

C:\PPMAC MiniGST\PowerPmac1\PowerPmac1\PowerPmac1.ppproj(176,5): Error : make: /bin/sh: Command not found

C:\PPMAC MiniGST\PowerPmac1\PowerPmac1\PowerPmac1.ppproj(176,5): Error : make: /bin/sh: Command not found

C:\PPMAC MiniGST\PowerPmac1\PowerPmac1\PowerPmac1.ppproj(176,5): Error : make: /bin/sh: Command not found

Build Process For usralgo.ko has ended.

 

Build Process For usralgo.so has started.

Build Process For usralgo.so has ended.

 

Done building project "PowerPmac1.ppproj" -- FAILED.'

 

the errlog for the realtime routines - which i think this is linked to since it fails during the usralgo.ko build is as follows:

 

'make: /bin/sh: Command not found

cp: missing destination file operand after '/usr/local/usralgo/usralgomain.c'

Try 'cp --help' for more information.

make: *** [all] Error 1'

 

as far as I am aware this usralgomain.c is a default file that has not changed between the two computers,

 

if anyone has seen this error before, and can point me in the right direction as to what I am doing wrong, it would be appreciated,

 

Colin

Link to comment
Share on other sites

  • Replies 1
  • Created
  • Last Reply

Top Posters In This Topic

Popular Days

Top Posters In This Topic

Guest
This topic is now closed to further replies.

×
×
  • Create New...