daves Posted May 30, 2017 Share Posted May 30, 2017 Hi I thought I would give the v3 IDE a whirl. Very excited about the new shell. I was asked to install 465 compiler on trying to build. But, our project does not build. Neither does a blank project with usrcode active: IDE3Test.ppproj(89,5): error : Makefile:327: /opt/powerpc-465-rootfs/usr/src/linux-3.2.21-serengeti-smp/scripts/Kbuild.include: No such file or directory IDE3Test.ppproj(89,5): error : /bin/sh: /opt/powerpc-465-rootfs/usr/src/linux-3.2.21-serengeti-smp/scripts/gcc-goto.sh: No such file or directory IDE3Test.ppproj(89,5): error : make: *** empty variable name. Stop. Indeed kbuild.include and gcc-goto.sh (in fact the whole scripts folder) are not present. They are present on a v2 install. What went wrong? What should I do? EDIT: A full reinstall didn't fix. It might help to know 460 and CK3E build without error. A quick run in WinMerge between v2 and v3 compilers clearly shows the missing files for 465. Cheers Dave Link to comment Share on other sites More sharing options...
steve.milici Posted May 31, 2017 Share Posted May 31, 2017 Please contact our Technical Support Group at support@deltatau.com with the PC and OS details. Link to comment Share on other sites More sharing options...
kmonroe023 Posted June 19, 2017 Share Posted June 19, 2017 Was there any resolution to this? I am having the same problem with a new V3 install. I did contact technical support on Friday, but I have not heard back from them yet. Hoping that pinging the problem here will help. For what it is worth, I was running V2 IDE with no issues. When I installed V3 I was not able compile c-code for the 465 processor. Other than the problems with not being able to compile, I liked the new shell. Overall it seemed snappier and and I really like that intellisense works offline now! I have a laptop running Win7 Enterprise 64bit, with 16G ram. Regards, kmonroe Link to comment Share on other sites More sharing options...
steve.milici Posted June 20, 2017 Share Posted June 20, 2017 The Software Development group is working on a patch for this. Link to comment Share on other sites More sharing options...
kmonroe023 Posted June 20, 2017 Share Posted June 20, 2017 The Software Development group is working on a patch for this. Perfect...thanks for the update. Link to comment Share on other sites More sharing options...
Faraday MC - Tony Posted June 21, 2017 Share Posted June 21, 2017 Try this. Go to C:\DeltaTau\PowerPMAC\Compilers\Installers\PowerPC465 and run setup. It will install the 465 compiler. I hope it works for you too! Link to comment Share on other sites More sharing options...
Recommended Posts