Jump to content
OMRON Forums

Recommended Posts

Posted

Hello there,

 

My CK3E firmware is 2.3.2.5.

I found it difficult to issue "ECAT[0].Enable=1" in terminal. I have downloaded the ENI file and setup motors and once successfully command motors to move. But if I issue "ECAT[0].Enable=0" and "$$$" then "ECAT[0].Enable=1", no motor movement can be found from Position window. Even "ecat reset" and "ecat slaves" cause no responce.

I'm sure ethercat network configuration is already downloaded.

The only way that make sense is to reboot CK3E and all slaves. All occurs again if CK3E is reseted..

 

Why?

  • Replies 2
  • Created
  • Last Reply

Top Posters In This Topic

Popular Days

Top Posters In This Topic

Posted
after you load the new firmware you must issue $$$*** then save the $$$. Then you must redownload the project and all motor settings. Then open system setup and redownload the .eni file. Again do a save and power cycle the slaves and the CK3E
Posted

after you load the new firmware you must issue $$$*** then save the $$$. Then you must redownload the project and all motor settings. Then open system setup and redownload the .eni file. Again do a save and power cycle the slaves and the CK3E

 

By saying "Again do a save and power cycle the slaves and the CK3E", you mean a reboot operation for CK3E and all slaves MUST be done after the save operation of downloading ENI file ?

 

I will have a try.

 

Thank you so much.

Guest
This topic is now closed to further replies.

×
×
  • Create New...