MattReid Posted January 4, 2018 Share Posted January 4, 2018 Hi, Just wondering the best way to clear an axis handwheel offset if setting the input to the master to zero didn't work. Usual Method (axis 3): We override a motion path by enabling master following I306=3 and then inputting an offset into the address defined by I305. (This goes through an exponential filter in ECT). To clear the offset we usually set the offset input to 0 which moves M367 back to 0. Problems (crash): There are times that setting the input to the filter to 0 doesn't totally clear M367. Therefore the present master position has an offset. What is the best way to get rid of the offset in M367? I tried to turn off following I306=0, then #3PMATCH, then write M367=0 which caused the axis move very fast but it clears it. I won't to avoid this rapid movement but totally clear the present master position. What is the recommended approach. Thanks Matt Thanks Matt Link to comment Share on other sites More sharing options...
Omron Forums Support Posted January 17, 2018 Share Posted January 17, 2018 #3HMZ should work. Link to comment Share on other sites More sharing options...
Recommended Posts