Jump to content
OMRON Forums

Position Compare with PFM Following Direct Micro-stepping


dhidas

Recommended Posts

Hello,

 

I am using direct microstepping on #1 of a GeoBrick LV and wish to use the position compare functionality as a trigger of sorts (in this case step as there is no encoder). I setup #5 as a virtual motor following the instructions for PFM so that I could use the position compare on #5 when it is following #1. The problem I am currently having is that #5 lags significantly behind #1 at higher speeds. I tried setting program acceleration and velocity to high values, the s-curve and accl-times to very small values for #5, and upped the PFM frequency, but I see no change in the amount of following error. Is there any other way to make #5 more synchronized with #1?

 

Thanks for your help,

 

-Dean

Link to comment
Share on other sites

  • Replies 1
  • Created
  • Last Reply

Top Posters In This Topic

Top Posters In This Topic

Can you jog #5 at the desired speed? If not what is the speed you get with #5O50 for example?

What settings did you use for motor #5 (including Gate settings)?

You should be able to set up a virtual PFM motor to run much faster than an actual motor. The driving clocks are PFM and encoder sampling frequency.

Link to comment
Share on other sites

Guest
This topic is now closed to further replies.

×
×
  • Create New...