d.manzenberger Posted April 4, 2018 Share Posted April 4, 2018 So we're setting up a machine to use a Power Brick with a Siemens PLC. We have the 72EX card installed, but I can't figure out for the life of me how to set it up for Profinet! I've read the manual, and it just looks like handwaving unless you're setting up ENIP. I was encouraged to read about a "ACC-72EX Setup Assistant Software", but was unable to locate it, and I can't tell if that would even be of use to me. Has anyone here set one up for Profinet, or does anyone know what that would look like? Thanks everyone! Link to comment Share on other sites More sharing options...
tecnico Posted April 6, 2018 Share Posted April 6, 2018 I use it with another bus (cclink) but basically the ACC72EX is a "carrier" for a Hilscher communication module and interfaces the PPMAC to the module's DPRAM On the manual is a ACC72EX init PLC and date exchange script PLCs, but you still have to program the Hischer ComX with Sycon.net AFAIK Link to comment Share on other sites More sharing options...
d.manzenberger Posted April 6, 2018 Author Share Posted April 6, 2018 I use it with another bus (cclink) but basically the ACC72EX is a "carrier" for a Hilscher communication module and interfaces the PPMAC to the module's DPRAM On the manual is a ACC72EX init PLC and date exchange script PLCs, but you still have to program the Hischer ComX with Sycon.net AFAIK So I've got the Sycon.net open, and I don't see any reference to an ACC-72EX device. How did you get that talking? Link to comment Share on other sites More sharing options...
tecnico Posted April 9, 2018 Share Posted April 9, 2018 Sycon doesn't talk to ACC72Ex but only to the module mounted on the ACC72Ex (Hilscher COM-C or COM-X) vua the micro usb port in the front panel of the ACC72EX. On the PMAC side there is a example PLC in the manual that enables data communication between the module and the host system (PMAC) Link to comment Share on other sites More sharing options...
Recommended Posts