shane Posted May 10, 2018 Share Posted May 10, 2018 In powerpmac,after I used data gather function ,such as : Gather.enable=2 x10 x20 Gather.enable=0 Can I export the gather data as a *.txt file or other file format for outside use.Not use the powerpmac ide's ploting funtion. Link to comment Share on other sites More sharing options...
steve.milici Posted May 10, 2018 Share Posted May 10, 2018 Yes - you can use the "gather_csv" executable from the Linux prompt using the "-u" with a filename option: gather_csv [-u] [filename] The “-u” will without the filename parameter will stream the contents of the most recent data gather to the standard output as in the current SSH, Telnet or serial port connection. The “-u” with the filename parameter will stream it to that file. Using the “/var/ftp/usrflash/” directory is recommended as this is already writable and will allow ftp uploads without any permission changes. For example: gather_csv -u /var/ftp/usrflash/mygatherfile This puts the last gathered data in a text file named “mygatherfile” in the “/var/ftp/usrflash/” directory where ftp access is available. Link to comment Share on other sites More sharing options...
shane Posted May 14, 2018 Author Share Posted May 14, 2018 Yes - you can use the "gather_csv" executable from the Linux prompt using the "-u" with a filename option: gather_csv [-u] [filename] The “-u” will without the filename parameter will stream the contents of the most recent data gather to the standard output as in the current SSH, Telnet or serial port connection. The “-u” with the filename parameter will stream it to that file. Using the “/var/ftp/usrflash/” directory is recommended as this is already writable and will allow ftp uploads without any permission changes. For example: gather_csv -u /var/ftp/usrflash/mygatherfile This puts the last gathered data in a text file named “mygatherfile” in the “/var/ftp/usrflash/” directory where ftp access is available. I wondered about what was written. The command is not gather_csv it is just gather. So you should do gather -u /var/ftp/gather/ggg.txt to send the already gathered data from the structures inside the ppmac to the file ggg.txt. I just tested this and it is working. My test was simple. I open the plot program and gathered some data and plotted it to be sure the gather worked. Then I ran the command and saw my file was created. Then I listed the file contents to verify it had the data inside. gather -u /var/ftp/gather/ggg.txt what is the difference between gather_csv and gather? Link to comment Share on other sites More sharing options...
shane Posted May 14, 2018 Author Share Posted May 14, 2018 i have tried system" gather -u /var/ftp/usrflash/sample.txt" and system"/opt/ppmac/gather_csv/gather_csv -u /var/ftp/usrflash/sample.txt",and they have the same effect, all creat a txt file named sample in /var/ftp/usrflash. but I still dont now why they are same. Link to comment Share on other sites More sharing options...
steve.milici Posted May 14, 2018 Share Posted May 14, 2018 The actual program is "gather_csv", "gather" is a symbolic link to be backwards compatible to older firmware. Link to comment Share on other sites More sharing options...
Recommended Posts