Jump to content
OMRON Forums

Geobrick Modbus TCP/IP client to ID 0 server not supported


sbrun

Recommended Posts

Dear All

 

I'm trying to power up the ModBus TCP/IP communication between Geobrick (Client) and RS232 to Modbus TCP/IP translator (Server).

But there is no way to have the communication OK because the server can't answer ModBus request with ID 0 that send the Geobrick.

Is there a way to change the ID number in the ModBus commande i67 + offset registers from 0 to 1 for example?

For memories the ModBus request are looking like:

ID + FC + Addr register + Length registers.

Today the Geobrick send 00 04 0014 0014 and the server would like to receive 01 04 0014 0014 ( ID 1, ModBus fonction 4, Start register address 20, and 20 registers read.

 

I was not able to find the answer in the "Modbus Definition and Design" documentation.

 

Many thanks for your help.

 

KR

Link to comment
Share on other sites

  • Replies 3
  • Created
  • Last Reply

Top Posters In This Topic

Guest
This topic is now closed to further replies.

×
×
  • Create New...