Jump to content
OMRON Forums

Problem Error .C


Eler0n

Recommended Posts

Hello. Please tell me how you can fix the error .C

With I have two identical Geo PMAC Drive GIL102M0 and both have the same error problem as in the photo.

 

At the same time, the + 3V lamp does not light up and the REG lamp lights up

 

There may be a nutrition problem. I fed the system with one phase 220v and three phases 380v each 136v But this did not work.

 

Could this mean that my GIL102M0 are not working and need repair? :(

20190822_143827.jpg.e8b307a7ba9c0b194ae5f77aa3664b7a.jpg

Link to comment
Share on other sites

  • Replies 6
  • Created
  • Last Reply

Top Posters In This Topic

Top Posters In This Topic

Posted Images

An error code of "C" is for an Under Voltage Fault. Here is the description:

The DC bus internal to the Geo drive has decreased below a factory pre-set threshold of 16 to 30Vdc (no AC input power to the drive).

 

To see other error messages, find "error codes" in the table of contents of this manual.

http://www.deltatau.com/manuals/pdfs/GEO%20PMAC%20DRIVE%20USER.pdf?id=635787783281109414

Link to comment
Share on other sites

Guest
This topic is now closed to further replies.

×
×
  • Create New...