RomanSolonto Posted November 13, 2019 Share Posted November 13, 2019 Good afternoon. We have the power pmac clipper board. We updated the firmware. We made an update through Power pmac IDE. During the update download, the connection was broken and the controller stopped loading. We checked the drive with the file system by loading it on a similar board, it was the pmac clipper board too. We think that the problem is the damage to the firmware of the FPGA. We tried to restore the firmware through USB. The controller does not read USB-drive. The controller also does not read the flash drive where the operating system (Linux) is located. We tried to create the folder "PowerPmacFactoryReset" on the USB drive and run the power pmac clipper. It doesn't work. Clipper didn't read USB-flash at all. Now when we start the clipper, it turns on green led and nothing more. Tell me how we can restore the boot firmware to turn the pmac clipper and fix board boot. Link to comment Share on other sites More sharing options...
Omron Forums Support Posted November 14, 2019 Share Posted November 14, 2019 Do you know if the firmware you installed was for a 465 CPU? If not, 465 firmware would need to be loaded before it will work. It is normal for the controller to reboot in the upgrade process, but it should come back afterwards. Are you specially power cycling PMAC with the USB inserted? Firmware would be replaced with a "PowerPmacFirmwareInstall" folder. See this forum post: http://forums.deltatau.com/showthread.php?tid=572 If you clipper does not boot properly, I would boot with a serial cable connected and send a log to ODT-Support@omron.com Can you tell me which firmware you were updating to which firmware? Link to comment Share on other sites More sharing options...
RomanSolonto Posted November 15, 2019 Author Share Posted November 15, 2019 The firmware version is 2-4-0-180. I tried to enable pmac with inserted usb disk (Folder PowerPmacFirmwareInstall was created). 2.1.1.3 powerpmac460ex from file depot. Nothing happens. Only green led and enabled fan. Link to comment Share on other sites More sharing options...
Alex Anikstein Posted November 18, 2019 Share Posted November 18, 2019 Roman, The Power Clipper is a 465 CPU, not a 460. Please try again using the "2.1.1.3 powerpmac465.zip" or "powerpmac465 2-4-0-180.zip" file from the File Depot, depending on which version you wanted to load. Link to comment Share on other sites More sharing options...
RomanSolonto Posted November 21, 2019 Author Share Posted November 21, 2019 I tried to create "PowerPmacFirmwareInstall" folder and put powerpmac465 2-4-0-180.zip and 2.1.1.3 powerpmac465.zip (packed and unpacked). Nothing happens. Link to comment Share on other sites More sharing options...
steve.milici Posted November 22, 2019 Share Posted November 22, 2019 The installation package "powerpmac.deb" file should be placed in this folder not the “zip” file. See the section “Special Power-On/Reset Modes” in the “Power PMAC User’s Manual” for a complete description: “http://forums.deltatau.com/filedepot/download.php?f=Power PMAC/Manuals/Power PMAC Users Manual.pdf” Link to comment Share on other sites More sharing options...
Recommended Posts