maxvoxel8 Posted April 5, 2021 Share Posted April 5, 2021 It seems that there is a bug when uploading a 2D comp table to the editor, editing it, and then downloading it. Sometimes the CompTable[x].X0[1] value gets reset to 100, and the CompTable[x].Ctrl value gets reset to 7 (I have it set to 23 normally). This bug is present in IDE 4.4.0.99. Link to comment Share on other sites More sharing options...
Omron Forums Support Posted April 5, 2021 Share Posted April 5, 2021 I am having trouble replicating the issue. Are you sure there aren't other settings somewhere in the project? 100 does not sound like a default value. You can try to CTRL+F and search the whole project or solution for the setting. Link to comment Share on other sites More sharing options...
maxvoxel8 Posted April 5, 2021 Author Share Posted April 5, 2021 I believe the problem may be in uploading. If I define a 2D comp table, download, then set Comptable[0].Ctrl to 23 in the terminal and then upload and download again, Ctrl gets reset to 7. Same with First Data Point 2, if I set it to 2000, and download, it works. But then if I reopen the editor and upload, it shows 100 for First Data Point 2. Also if I change the value Comptable[0].X0[1] in the terminal and upload, it doesn't update the value. This is on a Clipper with firmware 2.4.0.180, but it also shows up on a Powerbrick with 2.4.0.180 or 2.5.1.2. Link to comment Share on other sites More sharing options...
Smakarem Posted April 5, 2021 Share Posted April 5, 2021 Hi Max, I have replicated your issue with Ctrl getting reset to 7 as you described. I will bring this up with the software team and ask them to investigate further. Regards, Shadi Link to comment Share on other sites More sharing options...
illop Posted October 19, 2021 Share Posted October 19, 2021 add IDE 4.4.1.7 2D- compensation rollover "false" comptable[m].ctrl = $4 It will be $14. Link to comment Share on other sites More sharing options...
Omron Forums Support Posted October 22, 2021 Share Posted October 22, 2021 We are aware there are bugs and issues with the current Compensation Table tool. The April release will resolve these issues. Link to comment Share on other sites More sharing options...
Omron Forums Support Posted November 5, 2021 Share Posted November 5, 2021 In the future, please report bugs to the local support team, they submit them directly to the factory Link to comment Share on other sites More sharing options...
Recommended Posts