tkb11 Posted August 5, 2021 Share Posted August 5, 2021 I have a simple 3 line NC file. It has nothing but 'G00' on the first line. When I run it nothing happens. I suspect I need to do something to make G-Codes, even the default, work? Help? This is version 1.7r from 8/20/18. I've been successfully running programs from IDE version 4.4.2.3 but need to get NC16 working. The position display works. I can jog successfully and home works. The machine is very simple, a diamond turning machine with only two axis but uses interferometers for position (accurate to 1,270,000 counts per inch) TIA Link to comment Share on other sites More sharing options...
chrisvk Posted August 6, 2021 Share Posted August 6, 2021 May need to check coordinate system settings. I know cycle wont start if motors aren't closed loop and homed. Link to comment Share on other sites More sharing options...
Omron Forums Support Posted August 6, 2021 Share Posted August 6, 2021 G00 should just go into rapid mode, not actually move anything. What are the other 2 lines? Link to comment Share on other sites More sharing options...
tkb11 Posted August 6, 2021 Author Share Posted August 6, 2021 This is the entire program G00 X.1 F.1 M30 IDE (status dialog) says the motors are running closed loop and I can jog from within the IDE and from NC16. Do I need a script file to handle the G-Codes? The guy before me setup coordinate system 1, not 0. And used motor 1 and 2 instead of 0 and 1. Does that matter? I'm kinda fishing for answers ... Link to comment Share on other sites More sharing options...
Omron Forums Support Posted August 6, 2021 Share Posted August 6, 2021 The first line should just switch to rapid move, but not move anything. The second line should move X either to 0.1 or by 0.1. You might want to add G90 or G91 to be sure. The third line is just end of program. Are you sure X doesn't move? What response do you get if you type the following into the IDE terminal? #1-> The guy before me setup coordinate system 1, not 0. And used motor 1 and 2 instead of 0 and 1. Does that matter? That's normal and expected. Link to comment Share on other sites More sharing options...
steve.milici Posted August 6, 2021 Share Posted August 6, 2021 You need to load the supplied Project modified for your hardware. This contains the “script file to handle the G-Codes”. See the supplied documentation in the “Documents” folder for implementation details. Specifically: PowerPmacNC Quick Start_Ver6.pdf PowerPmacNC ini Configuraton Manual_Ver2.pdf PowerPmacNC Software Users Manual_Ver7-121217.pdf PowerPmacNC-Mill Manual_Ver3.pdf Link to comment Share on other sites More sharing options...
tkb11 Posted August 10, 2021 Author Share Posted August 10, 2021 Are you sure X doesn't move? positive - I can see the motors moving (or not moving) What response do you get if you type the following into the IDE terminal? #1-> &1#1->1270000x Link to comment Share on other sites More sharing options...
tkb11 Posted August 10, 2021 Author Share Posted August 10, 2021 You need to load the supplied Project modified for your hardware. This contains the “script file to handle the G-Codes”. See the supplied documentation in the “Documents” folder for implementation details. Specifically: PowerPmacNC Quick Start_Ver6.pdf PowerPmacNC ini Configuraton Manual_Ver2.pdf PowerPmacNC Software Users Manual_Ver7-121217.pdf PowerPmacNC-Mill Manual_Ver3.pdf I do not see anything about G-Code script files that is not specific to the NC16 projects built from source. We are using the default project as recommended by DT. The equivalent instructions are not clear (or present). I'm a cross platform real-time software developer and with respect, the documentation is pretty obtuse. Edit: Found the gcode script was there but not active. Removed all the Y axis references (since it is a fancy lathe) and it is working Link to comment Share on other sites More sharing options...
Recommended Posts