hongluck Posted October 15, 2021 Share Posted October 15, 2021 Hello, I am currently working on Clipper PLUS T3 controller. It is an 8axis clipper . I am using amp 1,2,3 as a milling machine. I want to integrate the spindle to the PMAC Controller and require DAC output. From the thread below I setup I variables. Looked at this thread but could not find an answer http://forums.deltatau.com/showthread.php?tid=185&highlight=spindle+clipper Same as the thread I would like to use DAC output from axis 6. This is what I set I7100=1090 I7101=5 I7102=3 // Output Mode , PWM I7126=0 ; default // Maximum Output I669=1090 ; DAC limit 10 Vdc Then (I600=0 (motor not active)) M602=545 however it did not show 5V. From the manual I found out that output6A(amp6 a output) is pin #4 but is it correct? If I set I600=1 Other pins have Voltage according to the manual but pin 4, 5 is always zero. Can anyone help with this issue? Link to comment Share on other sites More sharing options...
Omron Forums Support Posted October 18, 2021 Share Posted October 18, 2021 Which manual are you referring to? What is Clipper PLUS T3 Controller? With I600 = 0, you do not need to set I669. Is M602 pointer correct? Did you download the suggested M variables? With I600=1, do you see voltage output with #6Ox command(s)? I am deleting the thread in the Power PMAC forum as this is a Turbo PMAC issue. Link to comment Share on other sites More sharing options...
hongluck Posted November 1, 2021 Author Share Posted November 1, 2021 Yes it is a Clipper Plus T3 Controller How can I check M602 is correct? , Yes I downloaded suggested M variables It is the same I do not see voltage output with #6O50 command Link to comment Share on other sites More sharing options...
Omron Forums Support Posted November 8, 2021 Share Posted November 8, 2021 To check if m602 is set up correctly, enter "m602->" in the terminal and check if output matches "M602->Y:$07810A,8,16,S". (Value taken from suggested M-Variables in Turbo Software Reference Manual). Out of curiosity, do you have access to any local support? Link to comment Share on other sites More sharing options...
Recommended Posts