Jump to content
OMRON Forums

Adding Additional Motor


bprall

Recommended Posts

So I am trying to add a rotation stage to an almost straight download NC16 Project with 3 linear axis.  When I go through the motor setup Test and Set it can activate the Motor seen by looking at PWM amplifier display but the Terminal cannot and neither will the tune tools (as they are sending terminal commands).  This makes me think I missed something simple I have to add to the PLC.

 

Link to comment
Share on other sites

  • Replies 4
  • Created
  • Last Reply

Top Posters In This Topic

Top Posters In This Topic

Posted Images

  • 2 weeks later...

I adjusted the info in the PowerPmacNC.ini to have 4 motors with X,Y,Z,A and assigned the Motors to 1,2,3,5.  I also set up the coordinate system for 5->A

What I found when going through the PLC for NC16 is that the spindle based commands are a mix of SpindleAxis variable and a ton of Motor 4 specific commands making it tough to use Motor 4 without a lot of recoding and checking. 

I added in the commands for Motor 5 and have almost got it working.  Currently I see that the R position displayed is not mapping to the right value but the DTG value is correct.

 

 

RvsDTG.jpg

Link to comment
Share on other sites

This A position issue seems to have been that the base NC16 files have the Positions ordered as X,Z,Y,B,C in the P assignments so I add A initial as P105 but the NC16 is looking at P103 for the 4th position so need to move the Aposition to P103.

Edited by bprall
Link to comment
Share on other sites

Join the conversation

You can post now and register later. If you have an account, sign in now to post with your account.

Guest
Reply to this topic...

×   Pasted as rich text.   Paste as plain text instead

  Only 75 emoji are allowed.

×   Your link has been automatically embedded.   Display as a link instead

×   Your previous content has been restored.   Clear editor

×   You cannot paste images directly. Upload or insert images from URL.


×
×
  • Create New...