Loc_luu Posted February 4, 2022 Share Posted February 4, 2022 I appreciate any suggestions and helps from community for the following codes for homing 2 motors. The current code used H/W limit sensors but I want to disable HW flag and use SW flags instead. I tried to set I197=1, I124=$20000, I7212=0, I7213=0, I113-32000 and I could not make it to work. Thanks for the help. I124=131073;729 I224=131073;730 M316=0;731 M317=0;732 M318=0;733 I7212=2;734 capture on rising edge of a flag for Motor1 I7222=1;735 capture on flag low for Motor2 I7213=1;736 use PLIM1 as flag(positive end limit) for Motor1 I7223=0;737 use HOME2 (home flag) as trigger flag I123=12;738 Home speed with positive direction for Motor1 I223=30;739 Home speed with positive direction for Motor2 I126=0;740 no home offset for Motor1 I226=0;741 no home offset for Motor2 M145=0;742 M245=0;743 HOME1,2;744 Homing for Motor1 and 2 WHILE(M145=0ORM245=0);745 END WHILE;746 I123=-12;747 Home speed with negative direction for Motor1 I223=-30;748 Home speed with negative direction for Motor2 I7212=1;749 I7222=10;750 M145=0;751 M245=0;752 I126=P126;753 P126=-10000 home offset for motor1 HOME1,2;754 Home move for motor 1 and 2 WHILE(M145=0);755 END WHILE;756 M318=1;757 I5211=50;758 WHILE(I5211>0);759 END WHILE;760 M318=0;761 WHILE(M413=0);762 END WHILE;763 I5211=14000;764 WHILE(I5211>0);765 END WHILE;766 M317=1;767 I5211=500;768 WHILE(I5211>0);769 END WHILE;770 M317=0;771 WHILE(M413=0);772 END WHILE;773 PSETX(P30)Y(P31);774 M313=0;775 M314=1;776 P273=M201;777 P264=M264;778 ENABLE PLC2,3;779 P211=1;780 CLOSE;781 OPEN PROG 103 CLEAR;784 PSETX(P30)Y(P31);785 CLOSE;786 OPEN PROG 111 CLEAR;789 M110=1;790 M111=0;791 M112=0;792 M115=0;793 M114=0;794 M113=1;795 I123=P123;796 P123=100 home speed with positive direction for motor1 I124=8519681;797 hardware limit I126=0;798 no home offset I7212=2;799 capture on rising edge of a falg I7213=1;800 using PLIM1 as flag (positve end limit) HOME1;801 Home move for Motor1 I123=-P123;802 P123=100 home speed with negative direction for motor1 I7212=1;803 capture on flag high I126=P126;804 home offset -10000 HOME1;805 Homing move for motor1 M118=1;806 I5211=50;807 WHILE(I5211>0);808 END WHILE;809 M118=0;810 DWELL5000;811 M117=1;812 I5211=565;813 WHILE(I5211>0);814 END WHILE;815 M117=0;816 I124=8388609;817 M113=0;818 M114=1;819 M110=0;820 I-variables I111=32000;25966 I112=16000;25967 I113=0;25968 I114=0;25969 I114=0;25969 I115=0.25;25970 I116=1000;25971 I117=10000;25972 I118=0;25973 I119=100;25974 I120=0;25975 I121=50;25976 I122=32;25977 I123=-12;25978 I124=$20001;25979 I125=$78200;25980 I126=-10000;25981 I127=0;25982 I128=50000;25983 I129=0;25984 I130=34800;25985 I131=1100;25986 I132=1100;25987 I133=9500;25988 I197=0; I1711=32000;27566 I1712=16000;27567 I1713=0;27568 I1714=0;27569 I7211=0;33066 I7212=1;33067 I7213=1;33068 I7214=0;33069 Quote Link to comment Share on other sites More sharing options...
Gregs Posted February 16, 2022 Share Posted February 16, 2022 For homing, without absolute feedback, the axis must be moved to a position where an input is triggered to indicate an absolute position. Software alone cannot determine an absolute position. With software, the home position can be set equal to the current position using the HMZ command. Quote Link to comment Share on other sites More sharing options...
Recommended Posts
Join the conversation
You can post now and register later. If you have an account, sign in now to post with your account.