kmonroe023 Posted August 18, 2022 Share Posted August 18, 2022 Hello, I recently attempted to upgrade the FW on a 465 PMAC processor and discovered that the ethernet ports will no longer start at boot after the update. I can connect via the serial port and start the ethernet ports using ifup, so I think the network config in interfaces is ok. Once I start the eth ports I can connect using the IDE. Once connected, the FW update appeared successful and I was able to download and run my project. If I reboot or power down the processor, I have to connect serially to get the eth port running again. Running IDE V 4.5.2.9 Interfaces file attached. I've tried to flash it back to 2.5.0.4 and 2.4.0.180 to see if the network issue would fix itself; it didn't. Eth ports started at boot with both versions of FW before the 2.5.20 update. Any idea how to fix this? I assume some startup script isn't working correctly, but I'm not familiar with Linux so I don't know how to proceed. Thanks, kmonroe interfaces Quote Link to comment Share on other sites More sharing options...
steve.milici Posted August 18, 2022 Share Posted August 18, 2022 The 465EX PPC CPU is now obsolete. It was not fully tested on these newer FW versions. Contact the support group (ODT-Support@Omron.com) with your CPU SN. They can send you an image file to get back to 2.5.0.4. This was the last “fully” tested FW for 465. Quote Link to comment Share on other sites More sharing options...
kmonroe023 Posted August 19, 2022 Author Share Posted August 19, 2022 I figured it was something like that. I'll email support. Thanks, kmonroe Quote Link to comment Share on other sites More sharing options...
Recommended Posts
Join the conversation
You can post now and register later. If you have an account, sign in now to post with your account.