jayshah15028 Posted January 22 Share Posted January 22 Hi, I have a Power PMAC UMAC type controller with which I am communicating via ethernet protocol and trying to setup a voice coil motor with an analog linear encoder. I am using the motor setup topology in which I entered the amplifier information and voice coil information. But, 1. When I get to the encoder block, I enter the information and as soon as I click on Save, a connection error shows up (see image "connection_error"). Thereafter, in order to save these changes, I would have to click on connection setup and re-establish the connection between the Power PMAC and IDE (which shows connected all this time, even when the connection error pops up), and only then it allows to save the encoder block parameters. Also, this does not save in the true sense, because if I close and reopen the IDE, all the motor parametes and amplifier parameters along with hardware interface block parameters seem to be saved, but the encoder block does not get saved. 2. After (temporarily) saving the encoder parameters. when I get to the interactive feedback block, I do not see any signal from the encoder. I am not sure what the problem is. Your help is really appreciated. Thanks. Quote Link to comment Share on other sites More sharing options...
Eric Hotchkiss Posted January 27 Share Posted January 27 It sounds like 1 is the real issue and 2 happens because encoder settings aren't properly saved. Can you please share...? Your IDE version, firmware version, and CPU type. (in the green bar at the top of the IDE) A screenshot of the encoder setup page. A screenshot of the motor setup topology page. Quote Link to comment Share on other sites More sharing options...
jayshah15028 Posted January 27 Author Share Posted January 27 Hi Eric, Thanks for your reply. Please find the attached images. Quote Link to comment Share on other sites More sharing options...
Eric Hotchkiss Posted January 28 Share Posted January 28 This would be a technical support issue.Please contact ODT's direct technical support with your full issue details at:ODT-Support@Omron.comYou can also contact Omron TSG at "ia.techsupport@omron.com" but make sure to have PMAC or Delta Tau in the subject line for proper routing. Quote Link to comment Share on other sites More sharing options...
jayshah15028 Posted January 28 Author Share Posted January 28 Will do that. Thank you for the suggestion. Quote Link to comment Share on other sites More sharing options...
Recommended Posts
Join the conversation
You can post now and register later. If you have an account, sign in now to post with your account.