Jump to content
OMRON Forums

Onsys_JHLEE

Members
  • Posts

    5
  • Joined

  • Last visited

Recent Profile Visitors

274 profile views

Onsys_JHLEE's Achievements

Newbie

Newbie (1/14)

  • One Year In
  • One Month Later
  • Week One Done
  • First Post
  • Conversation Starter

Recent Badges

0

Reputation

  1. I have same issue. The symptoms of ECAT stopping often occurred when executing "ECAT RESET" in the IDE and then closing the IDE.
  2. Okay I will contact OEK. Thanks.
  3. Hi CK3M(2.6.1.0) IDE(4.6.0.14) EtherCAT slave - CDHD2 EtherCAT master stopped when I close PowerPMAC IDE. for detail - 1) "ECAT RESET" send command using terminal. 2) finish setup 3) Servo on EtherCAT motor. 4) close IDE Close IDE after using the "ECAT RESET" command as shown in the above procedure, The EtherCAT master stop. Without "ECAT RESET" That is okay. No problem. A similar phenomenon has occurred in several companies. That's all I've identified. It seems that the cause of this problem needs to be found and corrected. Thanks
  4. Thanks you reply. Change "Sys.NoShortCmds=1" seems to have more to lose than before. Is it difficult to automatocally read array variable from IDE? Thanks jaehyuk
  5. Hi Some time Some motor not moving because coordinate feed 0%. This problem is reproduced in the following situations: - Incorrect command is issued to show the value of array data 'h' is included in the name of the array , and is recognized as this "Hold" command. - It is same when I using terminal ( feed will go to zero) So I didn't use parameter information. but the function is very useful. Is there a solution? Thank you. jaehyuk
×
×
  • Create New...