About the tab 'Kernel update' in the IDE, some questions :
- Button KERNEL: When click it is proposed to save the OS on the PC in uImagebackup10222010.bin
But it doesn't success ant it says 'File{0} transfer error'
Do i have to add jumpers on the CPU board ?
- Could you explain how to use the Kernel update possibilities ?
(button Kernel, Boot, Install package) and what files to use.
Do i have to connect under linux for the install of the files : usr.tar.gz, partition2.tar.gz and use those commands :
cd /var/ftp/usrflash
mount -o remount,rw /
tar xfz usr.tar.gz
cp -a usr /
mount -o remount,ro /
is it correct ?
PS: I work with: Kernel version 2.6.30.3, Firmware PPmac 1.2.1.5 and IDE 1.1.2.45, but those questions are for my customers and the future.