sbrun
-
Posts
58 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by sbrun
-
-
Thank you for your answer. I checked the configuration and it is exactly as you said (with an additional \2.0\ as : ...System Inc\2.0\Power PMAC Suite ...) My Pb stay the same ... I uninstall and reinstall without any evolution.
-
I just upgraded with Firmware PPmac 1.2.1.5 and IDE 1.1.2.45 + SP2 (32bits) I simply create a new projet in the IDE with the template: "PowerPmac" When i build it, i got 73 error messages : "Error :Reside in x:\cygwin\bin, where 'x' is the drive on which you have" in file:PowerPmac1.ppproj line:106 column: 6 I don't success to fix it ? (Same errors with all my old projects)
-
About the tab 'Kernel update' in the IDE, some questions : - Button KERNEL: When click it is proposed to save the OS on the PC in uImagebackup10222010.bin But it doesn't success ant it says 'File{0} transfer error' Do i have to add jumpers on the CPU board ? - Could you explain how to use the Kernel update possibilities ? (button Kernel, Boot, Install package) and what files to use. Do i have to connect under linux for the install of the files : usr.tar.gz, partition2.tar.gz and use those commands : cd /var/ftp/usrflash mount -o remount,rw / tar xfz usr.tar.gz cp -a usr / mount -o remount,ro / is it correct ? PS: I work with: Kernel version 2.6.30.3, Firmware PPmac 1.2.1.5 and IDE 1.1.2.45, but those questions are for my customers and the future.
-
I need to run very large programs which are on the hard disk of the PC. I intend to use the rotary buffer to send it. On the forum, i found only an information (post by BradP 04-05-2010) supposing that the program file was already in the Linux area on the PPmac. Have you an example of code running on Windows (c#, visualBasic,...) to send and run a big program file ? Thanks
-
Really, neither : Prog[n].Ldata.L[n] or Plc.3.MyVar seems to work. Is there something else to do to see local variables ?
-
How to Stat/Stop the Gathering from the inside of a running program. Like as the Turbo commands GATHER, END GATHER, DEL GATHER, ...
-
Usually I use Pewin32 under an administrator account. How to use it under a user (no administrator) account with XP-sp3, with Vista ?
Errors : in x:\cygwin\bin ??
in Power PMAC
Posted