andreychip
-
Posts
54 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by andreychip
-
-
See attachments.
Thank you. But I asked for the code for ACC-24S3 for boards Power Clipper .
-
Hi.
I wanted to know the order code for ACC-24S3 4-Channel Axis Expansion Stack Board.
best regards Andrey.
-
thank you very much
-
What to do with the files in the firmware and ppmac.zip sourcediff.zip ?
-
thank you very much
-
You can get new firmware on the PowerPmac Clipper controller and the instructions how to sew.
-
What is the response to the "vers" command?
a task manager screenshot
-
Hello.
We have a PowerClipper firmware version 2.0.2.14.
Working with PoverIDE version 2.0.3.40 4/21/2015,
no problem, attached screenshots .
When you install the new PowerClipper version 2.2.0.39 7/16/2016 we had a problem with the configuration EtherChat:
9/9/2016 :9:46 AM - 192.168.10.200, Module - Setup Motor : Error - EtherCAT setup requires a Firmware upgrade to version 2.0.2.210 or newer.
Attached screenshots below.
best regards.
-
thank you.
-
1.What delivery times NC14 in russia?
2.How many axis available for Russia?
-
The settings are correct. They assume a “standard” ECT setup (created in ENCODER.TAB):
(note that I have added the first four standard entries for completeness assuming Turbo PMAC2)
// Encoder Conversion Table for Lathe with standard 1/T feedback type.
// For any other feedback device user will have to change this file for
// Lathe FPR mode to work Correctly.
// Typical Lathe Motor 1, 3 and 4.
// we will add 4 dummy entries in Encoder table.
//---------------------------------------------------------
//I8000=$78000 //$3501
//I8001=$78008 //$3502
//I8002=$78010 //$3503
//I8003=$78018 //$3504
I8004=$78100 //Dummy ECT Entry 4 $3505
I8005=$78108 //Dummy ECT Entry 5 $3506
I8006=$78110 //Dummy ECT Entry 6 $3507
I8007=$78118 //Dummy ECT Entry 7 $3508
I8008=$403504 //$3509
I8009=$64 //$350A
I8010=$A78018 //$350B
I8011=$F5C //$350C
I8012=0
If you have modified the ECT to have a different structure then you will need to edit this file.
I8010=$A78018 //$350B
The bit 19 mode switch must be set to 0 if a PMAC-style Servo IC (DSPGATE)
is addressed; it must be set to 1 if a PMAC2-style Servo or MACRO IC (DSPGATE1 or DSPGATE2) is addressed. Note that setting bit 19 to 1 changes the second hex digit of the I-variable from 7 to F. TurboSRM page 240.
I8010=$AF8018.
-
Check spindle parameter in the registry NC Pro 2 encoder counts 4096 was installed.
-
Hi. I can give the manual Power PMAC-NC HMI (PPNC), please?
-
Thank you.
-
Hi.
Do not prompt, Power PMAC-NC16 works with TURBO CLIPPER ?
Thank you!
-
Hi.
You can tell the price Power PMAC NC 14 Software Development Kit (Two Runtime Licenses Included) PPNC-0000000-002-000 for Russia?
Thanks.
-
These file come as part of the Renishaw product installation.
Thank you for your help
-
Hi. Where to get these files
Files Required for Installation
Renish.pmc FANUC to PMAC translated probing routines.
Probe.plc Initializes probe, monitors skip signal.
Errors.dat Contains text of alarms specific to probing.
Dprnt.enu ?
-
we use PHMI-NC-PRO2.
Thanks, at the moment everything is working
-
Hi !
May specifically describe what this Alarm "(X) Motor on limit"?
This type of alarm occurs, when the load on the drive increases .
-
text message "(X) Motor on limit"
Alarm eliminated reduced parameter I117 from 0.2 to 0.1
-
hi!
The problem is that when turning on the details of the function G01 there is an alarm "motor on limit" and stop the drive.
What kind of alarm?
How to find the cause of this alarm?
thank you
-
Hello there
In my software, it extracts dxf files into set of trajectories data for the entire profile, which consists of position X, position Y, Speed, IJK values (for circular trajectories), Move Type(linear, circular, arc or spline).
Currently i am command the XY Axis moves interpolation point by point where the pmac code was very simple of moves interpolation, decelerate, and stop, then for the next point of the trajectory to complete an entire profile.
However this gives unsatisfied output of quality which required to moves entire profile without decelerates and stops.
I'm considering using the Q variables, but then what if the number of position X&Y and other parameters exceed the number allowance of variables? and do you have a sample of pmac code or similar case to study or reference?
How do i throw in all the trajectories data (position, type of moves, speed, and ijk value) as buffer and it runs the entire profile in the pmac program but not command by command from my software?
Thank You
Best Regards
Terry
Read guide TURBOPMAC_USER_MANUAL and TURBO SRM
http://www.deltatau.com/Manuals/Default.aspx
example ROTARY buffer
-
see description of ACC-36E http://www.deltatau.com/Manuals/Default.aspx
Part Number for ACC-24S3 Axis Expansion Stack Board
in Power PMAC
Posted
Thank you.