Jump to content
OMRON Forums

How many counts(The max position) can Turbo arrive?


dzrong

Recommended Posts

  • Replies 3
  • Created
  • Last Reply

Top Posters In This Topic

Top Posters In This Topic

If you are only jogging a motor the motor will behave in a controlled fashion as the position registers roll over. For axis moves in a C.S. this will result in a serious condition though as the axis definitions will be using the wrong value in motor position – you will probably get a fatal following error.
Link to comment
Share on other sites

If it is just a motor move rolling over between maximum positive and negative values (in either direction), there will be no problem in operation.

 

However, if the motor is moving because it is assigned to an axis, and the motor position rolls over because the matching axis position goes out of the motor range, you will get a fault because the math cannot work out to a proper position.

 

It is a very rare Turbo PMAC application where this is even a potential problem. Reducing Ixx08 in these applications extends the real range proportionately.

Link to comment
Share on other sites

Guest
This topic is now closed to further replies.

×
×
  • Create New...