kandauru Posted December 26, 2014 Author Share Posted December 26, 2014 Hi, I am trying to use rotary buffer in my application to move axes. But the problem is that axes are not moving at all. All axes are homed and enabled. Please, advise, what is wrong. The following lines of source code are how I am trying to do that: &1a Define rotary BUFFER_SIZE open rotary Coord[1].MaxFeedrate = FEEDRATE Coord[1].Tm = -SPEED x-283.000 Y202.000 Z305.000 V90.000 U-84.000 x-285.000 Y202.000 Z305.000 V93.000 U-84.000 x-287.000 Y202.000 Z305.000 V96.000 U-84.000 x-289.000 Y202.000 Z305.000 V99.000 U-84.000 x-290.000 Y202.000 Z305.000 V100.000 U-84.000 x-289.000 Y202.000 Z305.000 V99.000 U-84.000 x-287.000 Y202.000 Z305.000 V96.000 U-84.000 x-285.000 Y202.000 Z305.000 V93.000 U-84.000 x-283.000 Y202.000 Z305.000 V90.000 U-84.000 close &1b0r Link to comment Share on other sites More sharing options...
kandauru Posted December 26, 2014 Share Posted December 26, 2014 Hi, I am trying to use rotary buffer in my application to move axes. But the problem is that axes are not moving at all. All axes are homed and enabled. Please, advise, what is wrong. The following lines of source code are how I am trying to do that: &1a Define rotary BUFFER_SIZE open rotary Coord[1].MaxFeedrate = FEEDRATE Coord[1].Tm = -SPEED x-283.000 Y202.000 Z305.000 V90.000 U-84.000 x-285.000 Y202.000 Z305.000 V93.000 U-84.000 x-287.000 Y202.000 Z305.000 V96.000 U-84.000 x-289.000 Y202.000 Z305.000 V99.000 U-84.000 x-290.000 Y202.000 Z305.000 V100.000 U-84.000 x-289.000 Y202.000 Z305.000 V99.000 U-84.000 x-287.000 Y202.000 Z305.000 V96.000 U-84.000 x-285.000 Y202.000 Z305.000 V93.000 U-84.000 x-283.000 Y202.000 Z305.000 V90.000 U-84.000 close &1b0r Link to comment Share on other sites More sharing options...
Gregs Posted December 29, 2014 Share Posted December 29, 2014 Maybe a Clear Rotary command needs to be issued so that pre-existing lines in the buffer are not being unexpectedly executed. Is BUFFER_SIZE greater than 2048? Link to comment Share on other sites More sharing options...
Gregs Posted December 29, 2014 Share Posted December 29, 2014 Maybe a Clear Rotary command needs to be issued so that pre-existing lines in the buffer are not being unexpectedly executed. Is BUFFER_SIZE greater than 2048? Link to comment Share on other sites More sharing options...
steve.milici Posted December 30, 2014 Share Posted December 30, 2014 Also check for any motors in the CS not in closed loop. Link to comment Share on other sites More sharing options...
steve.milici Posted December 30, 2014 Share Posted December 30, 2014 Also check for any motors in the CS not in closed loop. Link to comment Share on other sites More sharing options...
kandauru Posted December 30, 2014 Author Share Posted December 30, 2014 Thank you for replies! 1) The buffer size is 4096. And may be greater. 2) All motors are in closed loop. But to get feedback I need them to be in closed loop. It looks like it moves, but very very slowly. Link to comment Share on other sites More sharing options...
kandauru Posted December 30, 2014 Author Share Posted December 30, 2014 Thank you for replies! 1) The buffer size is 4096. And may be greater. 2) All motors are in closed loop. But to get feedback I need them to be in closed loop. It looks like it moves, but very very slowly. Link to comment Share on other sites More sharing options...
Gregs Posted December 30, 2014 Share Posted December 30, 2014 Are the following set up correctly: Linear mode Coord[1].Ta, Coord[1].Td and Coord[1].Ts (Set time in acceleration, deceleration, and S-curve accel) Motor[x].MaxSpeed Frax (Use Frax command to choose which axes are used in vector feederate calculations) Link to comment Share on other sites More sharing options...
Gregs Posted December 30, 2014 Share Posted December 30, 2014 Are the following set up correctly: Linear mode Coord[1].Ta, Coord[1].Td and Coord[1].Ts (Set time in acceleration, deceleration, and S-curve accel) Motor[x].MaxSpeed Frax (Use Frax command to choose which axes are used in vector feederate calculations) Link to comment Share on other sites More sharing options...
curtwilson Posted January 5, 2015 Share Posted January 5, 2015 A "feedrate" value is a commanded vector speed of your "feedrate axes". The intent of this functionality is to get a constant tool-tip speed in 2D or 3D Cartesian space without the user having to compute the individual axis speeds. PMAC does this by first computing the vector distance of the feedrate axes by Pythagorean theorem, then dividing by feedrate to get the move time. By default, the "feedrate axes" are X, Y, and Z. It is possible to change this with the FRAX command, but very few people do (and I don't think you have changed this). The idea of a constant vector feedrate regardless of direction does not make geometric sense with more than 3 dimensions. In your example, your vector distance is zero. Since you also have "non-feedrate" axes (U and V), it instead computes the move time by dividing the commanded distance of each non-feedrate axis by the saved parameter Coord[x].AltFeedrate, and taking the largest of these times. The resulting motor speeds are then compared to Motor[x].MaxSpeed for each motor, with the move time extended if any of these limits are exceeded. So you first need to check your value of Coord[x].AltFeedrate, then the values of Motor[x].MaxSpeed as Greg said. Link to comment Share on other sites More sharing options...
curtwilson Posted January 5, 2015 Share Posted January 5, 2015 A "feedrate" value is a commanded vector speed of your "feedrate axes". The intent of this functionality is to get a constant tool-tip speed in 2D or 3D Cartesian space without the user having to compute the individual axis speeds. PMAC does this by first computing the vector distance of the feedrate axes by Pythagorean theorem, then dividing by feedrate to get the move time. By default, the "feedrate axes" are X, Y, and Z. It is possible to change this with the FRAX command, but very few people do (and I don't think you have changed this). The idea of a constant vector feedrate regardless of direction does not make geometric sense with more than 3 dimensions. In your example, your vector distance is zero. Since you also have "non-feedrate" axes (U and V), it instead computes the move time by dividing the commanded distance of each non-feedrate axis by the saved parameter Coord[x].AltFeedrate, and taking the largest of these times. The resulting motor speeds are then compared to Motor[x].MaxSpeed for each motor, with the move time extended if any of these limits are exceeded. So you first need to check your value of Coord[x].AltFeedrate, then the values of Motor[x].MaxSpeed as Greg said. Link to comment Share on other sites More sharing options...
curtwilson Posted January 6, 2015 Share Posted January 6, 2015 More precisely, if the time for any of the non-feedrate axes, as calculated by (AxisDistance/AltFeedrate), is greater than the time calculated for the combined vector feedrate axes (VectorDistance/Feedrate), it will use this longer time, and the actual vector feedrate used for the move will be less than what was commanded. Link to comment Share on other sites More sharing options...
curtwilson Posted January 6, 2015 Share Posted January 6, 2015 More precisely, if the time for any of the non-feedrate axes, as calculated by (AxisDistance/AltFeedrate), is greater than the time calculated for the combined vector feedrate axes (VectorDistance/Feedrate), it will use this longer time, and the actual vector feedrate used for the move will be less than what was commanded. Link to comment Share on other sites More sharing options...
kandauru Posted January 8, 2015 Author Share Posted January 8, 2015 Thank you for support! I am going to check all you said here. Link to comment Share on other sites More sharing options...
kandauru Posted January 8, 2015 Author Share Posted January 8, 2015 Thank you for support! I am going to check all you said here. Link to comment Share on other sites More sharing options...
Omron Forums Support Posted January 13, 2015 Share Posted January 13, 2015 I know this might be obvious, but have you actually defined axis definitions in coordinate system 1? For example: &1 #1->X #2->Y #3->Z #4->V #5->U Link to comment Share on other sites More sharing options...
Omron Forums Support Posted January 13, 2015 Share Posted January 13, 2015 I know this might be obvious, but have you actually defined axis definitions in coordinate system 1? For example: &1 #1->X #2->Y #3->Z #4->V #5->U Link to comment Share on other sites More sharing options...
JohnR Posted January 15, 2015 Share Posted January 15, 2015 I know this maybe a little off topic, however I’ve seen this issue several times in the forum and it’s happened to me many times. Is/could there be a way to determine the limiting parameter in a motion move? Link to comment Share on other sites More sharing options...
JohnR Posted January 15, 2015 Share Posted January 15, 2015 I know this maybe a little off topic, however I’ve seen this issue several times in the forum and it’s happened to me many times. Is/could there be a way to determine the limiting parameter in a motion move? Link to comment Share on other sites More sharing options...
curtwilson Posted January 15, 2015 Share Posted January 15, 2015 The best way to figure out what is going on is to plot the desired velocity profile through data gathering. There are many different limiting factors that could occur at different stages in the calculations. I don't think it would be feasible to flag all of them. Link to comment Share on other sites More sharing options...
kandauru Posted June 24, 2015 Author Share Posted June 24, 2015 Hi, I am facing a new problem using rotary buffer: the rotary buffer stops running after first line was executed. Please, advise how to fix this problem. Here is my source code: CS defined as below: &1 #1->x #2->0 //position follower of #1 #3->xx #4->0 //position follower of #3 #5->y #6->yy #7->z #8->zz #9->u #10->uu //#11->a //not used in current configuration //#12->aa //not used in current configuration //#13->b //not used in current configuration //#14->bb //not used in current configuration #15->v #16->vv Then in my application written on C#: //buffer initialization cmds.Add("&1a"); cmds.Add("&1 delete rotary"); cmds.Add("&1 define rotary " + ROT_BUF_SIZE); // ROT_BUF_SIZE = 4096 cmds.Add("&1open rotary linear abs close"); cmds.Add("&1b0r"); SendCommands(rotComm, cmds, out res); //buffer filling cmds.Add("&1open rotary X92028 Y1089221 Z1631730 U-500011 V173488 close"); cmds.Add("&1open rotary X92087 Y1089385 Z1636252 U-500125 V172850 close"); //at this line the execution stops cmds.Add("&1open rotary X92152 Y1089550 Z1640774 U-500238 V172212 close"); cmds.Add("&1open rotary X92221 Y1089714 Z1645296 U-500352 V171575 close"); cmds.Add("&1open rotary X92296 Y1089878 Z1649817 U-500465 V170937 close"); cmds.Add("&1open rotary X92376 Y1090042 Z1654338 U-500579 V170300 close"); cmds.Add("&1open rotary X92461 Y1090206 Z1658858 U-500692 V169662 close"); cmds.Add("&1open rotary X92552 Y1090370 Z1663377 U-500806 V169025 close"); cmds.Add("&1open rotary X92648 Y1090533 Z1667895 U-500920 V168387 close"); cmds.Add("&1open rotary X92749 Y1090697 Z1672411 U-501034 V167750 close"); cmds.Add("&1open rotary X92855 Y1090860 Z1676927 U-501147 V167112 close"); cmds.Add("&1open rotary X92966 Y1091024 Z1681440 U-501261 V166475 close"); cmds.Add("&1open rotary X93083 Y1091187 Z1685953 U-501375 V165837 close"); cmds.Add("&1open rotary X93205 Y1091350 Z1690463 U-501490 V165200 close"); cmds.Add("&1open rotary X93332 Y1091513 Z1694971 U-501604 V164563 close"); cmds.Add("&1open rotary X93464 Y1091676 Z1699478 U-501718 V163925 close"); SendCommands(rotComm, cmds, out res); Link to comment Share on other sites More sharing options...
steve.milici Posted June 25, 2015 Share Posted June 25, 2015 Check motor status and CS status- more than likely this is the cause - the program is being aborted or maybe stopped by a feed hold. Link to comment Share on other sites More sharing options...
kandauru Posted June 26, 2015 Author Share Posted June 26, 2015 I see in CS1 Error Status "RunTimeError". What to check? Link to comment Share on other sites More sharing options...
JohnR Posted June 26, 2015 Share Posted June 26, 2015 I see in CS1 Error Status "RunTimeError". What to check? Check the Error Status to determine what caused the RunTimeError Coord[x].ErrorStatus Power PMAC Software Reference Manual - Page 667 Link to comment Share on other sites More sharing options...
Recommended Posts