Jump to content
OMRON Forums

Power Pmac Develoment Kit and NC14


kjcho
 Share

Recommended Posts

  • Replies 14
  • Created
  • Last Reply

Top Posters In This Topic

Hi,

 

You get the examples when you buy the PDK. Assuming you're in Korea, you can buy it from DT Korea or Daekhon, whose contact information is here:

 

DELTA TAU KOREA

J.Y. Park

701-ho, Unitech Vil.

Baekseok, Ilsan, Koyang

Kyungki-Do 411-722

South Korea

Phone: 011 82-31-813-6156

Fax: 011 82-31-813-6155

dtkorea@deltatau.com

http://www.deltatau.com

 

 

DAEKHON CORPORATION

Mijin Song

1201 Ace Techno Twin Tower 1

212-1 Guro-Dong

Guro-Gu Seoul 152-050

Korea

Phone: 82 2 6675-6628

Fax: 82 2 6675-6644

std@daekhon.co.kr

http://www.daekhon.co.kr

Link to comment
Share on other sites

Note that our Power PMAC NC software was developed under a different platform not just with the PDK. You can purchase the NC software with the development platform:

Power PMAC NC 14 Software Development Kit (Two Runtime Licenses Included) PPNC-0000000-002-000

Site License, Redistributable, Runtime Licenses Required for deployment.

Link to comment
Share on other sites

The PDK is not designed to create an extensive program such as the PMAC NC 14. PMAC NC 14 includes many complex functions and would take a significant amount of time to re-create. If you need the functionality which is containted in NC14, but need to customize it, the Power PMAC NC 14 SDK could be a good solution.
Link to comment
Share on other sites

Here's 3 questions.

 

1. Is NC14 still under developing?

Why NC14 is not listed on deltatau.com?

 

2. I want to developement my own NC system using Turbo pmac or Power pmac and it would be used on 10~20 machines.

Is it possible to use NC software developed with NC14 SDK in that way?

What is 2-runtime license? Is license needed using my own software developed with NC14 SDK?

 

3. I found NC14 on the web but I have no information about it.

Can I ask NC14 manual or application example??

 

Thank you.

Link to comment
Share on other sites

  • 4 months later...
  • 8 months later...
Guest
This topic is now closed to further replies.
 Share


×
×
  • Create New...