Jump to content
OMRON Forums

Power PMAC Etherlite and Power Brick AC


MatthieuBarreau

Recommended Posts

Hi,

 

I am studying the Power PMAC Etherlite and Power Brick AC. I would like to link them together using MACRO, is the fiber inside the package ? If not I can't find the information about where one can find it.

 

I have also some (maybe really debutant) questions:

- We need a 24 VDC supply quite often, if we use only one for all the requirements (Brake Power, STO and for the Etherlite), do you have some advice on one specific generator supply to do so?

- What is the +24 VDC RET?

- Do one need to order all the connectors from Phoenix?

- Is there any website on which we can order all the D-sub needed?

 

I would like to use an encoder and the output signal is square signals but this is not digital. Should I use a ADC and then the Encoder X1 or can I use the analog input ?

 

Thank you in advance,

 

Matthieu

Link to comment
Share on other sites

  • Replies 14
  • Created
  • Last Reply

Top Posters In This Topic

The fiber optic cable is not included. You must order this separately.

 

No recommendations for the brand of 24VDC supply. You just must be sure of the current requirement remembering that all electronics such as encoders connected to the PowerBrick will also be powered from this supply. And of course you need to make sure you create no GND loops or other electrical problems.

 

Connectors do not need to come from Phoenix. But we have seen some low cost/quality connectors in which the internal contacts have a slightly smaller diameter and/or reach which cause intermittent connection problems. So whatever you select consider this.

 

We normally order from Distrelec.

 

I do not understand this question. The encoder has a square wave output or an analog output?

Link to comment
Share on other sites

So it is an incremental "quadrature" encoder. It has connection A B and index. A and B are square waves shifted by 90 degrees. C comes once per revolution.

 

If this is correct then this is the standard encoder input type.

Link to comment
Share on other sites

Yes it is, thank you very much.

 

I cannot find any information about the needed optical fiber. Is there a pdf document that I missed ?

 

EDIT : Ok, I just check the new manuals and it is clearly written. I assume it is SC for all devices. If I have only two devices connected each other, is a duplex possible to use ?

Link to comment
Share on other sites

I do not understand what you mean with buying a main power bus. But, The pBrick is a motion controller and amplifier in one box. amplifiers drive motors and need a bus supply for that purpose. The etherlite is just a motion controller so it only needs logic power. The amplifiers are external and not the concern of the etherlite.
Link to comment
Share on other sites

  • 2 weeks later...

Hi,

 

I am thinking of the power supply about the Main Power Bus.

There is a procedure for choosing the correct fuses in the manual (p42). The example given if for a AC motor, mine are DC, with a current of 1.6A at 6V, how should I choose the fuse?

I have another beginner question. How can I know the characteristic of the power supply knowing the motors I will use?

 

Thank you again,

 

Matthieu

Link to comment
Share on other sites

You would need to follow the same equations. Just make sure you calculate the individual elements in the equations according to what motor you are connecting. So so V_motorphase and P_axis will be calculated for your brush motor (which looks like a single phase motor) and not 3-phase motor.

 

Another question comes up. Why are you driving such a small motor with pBrick AC. It seems you should be using pBrick LV?

Link to comment
Share on other sites

Thank you for the advice.

 

Good question ;-) It is a test bench to show that pBrick AC can do the job the company want for bigger motors (Gemini Observatory). So I must do it with small motors first.

 

Another question: The documentation about the watchdog for pBrick AC is quite obscure. It is written 5 Pin TB, is there a N/P from Phoenix Contact or Delta-Tau order?

Link to comment
Share on other sites

Guest
This topic is now closed to further replies.

×
×
  • Create New...