AnthonyLH Posted August 7, 2015 Share Posted August 7, 2015 Hello, I cannot correctly mount an SD card on my current PPMAC. It the first time it is happening, i start a PPMAC every months... From my understanding, a FAT32 SD card, with no USB stick connected on the PPMAC, should be found at "/dev/sdb#" (the b of sdb# is important) and mounted automatically to "/media/disk-0" at start up thanks to the "/.readonly/etc/usbmount/usbmount.conf" file. On this specific PPMAC, the SD card seems to change of block name after or during the mounting: on the example screen shot, it is changing from "/dev/sdb5" to "/dev/sdc5" to "/dev/sdd5" and so on.. Does someone see a potential reason/origin for/to this behaviour? Thank you!! The explication below is how i placed the finger on the issue... on our standard application we use an ext3 SD card. ------- To mount an ext3 SD card on the PPMAC, i modify the "fstab" file (with "mount -o remount,rw /" cmd before and "mount -o remount,ro /" after). The line i added is "/dev/sdb1 /media/disk-0 auto defaults 0 0". On this specific PPMAC, the device block seems to change during the boot (changing from "/dev/sdb1" to "/dev/sdc1"). When i look in "mtab" ("cat /etc/mtab") i see that "/dev/sdb1" was mounted. When i send "blkid" is see that the device is now "/dev/sdc1". I did few other tests: -changed the "fstab" line to "LABEL=SD /media/disk-0 auto defaults 0 0" : i still see the "sdb1" in "cat /etc/mtab" and the "sdc1" using "blkid". -removed the line in "fstab" and modify "/.readonly/etc/usbmount/usbmount.conf" file. I added the ext3 to the line: "FILESYSTEMS="ext3 vfat"". After doing this i observed a multi-mount of the same device... it mount it, the device change (sdb1 to sdc1), it try to mount the new one and so on.. Link to comment Share on other sites More sharing options...
KEJR Posted August 12, 2015 Share Posted August 12, 2015 What do you get when you type "ls /dev/sd*" ??? On my system I have a SDcard plugged in with one partition on it (sdb1). # ls /dev/sd* /dev/sda /dev/sda1 /dev/sda2 /dev/sdb /dev/sdb1 sda is the builtin flash drive and sda1 and sda2 are the PPMAC partitions. sdb is the SDcard drive and, in my case, sdb1 is the first and only partition (it happens to be ext2 which is not important at this stage). If you see the same devices above you can edit the fstab file to mount /dev/sdb1 to a directory of your choosing. I created /mnt/sdcard on my system and have the following fstab file: # /etc/fstab: static file system information. # # proc /proc proc defaults 0 0 /dev/sda1 /opt vfat ro 0 0 /dev/sda2 / ext2 ro 0 0 /dev/sdb1 /mnt/sdcard ext2 rw tmpfs /tmp tmpfs defaults Just add the line, change the filesystem, and save to /.readonly/etc/fstab and reboot and you should be all set. the automounters are convenient for desktops and people plugging in thumb drives but on a system I prefer to mount it statically for determinism. If your device listing if off from mine then you may have a problem with the kernel recognizing your sdcard hardware. Let us know how it goes. Link to comment Share on other sites More sharing options...
AnthonyLH Posted August 13, 2015 Author Share Posted August 13, 2015 Thank you Kejr, For my standard projects i add the line "/dev/sdb1 /media/disk-0 auto defaults 0 0" in the "fstab" file. I used the automounter only this time to test. Recall of the issue: as soon as the SD card is mound, the block device change, the first change goes from sdb1 becomes sdc1. Without the autolounter, it stop there, so i have "sdb1" mounted but not present anymore. The device is present on "sdc1". Using the automounter, the new sdc1 is detected and mounded and then directly changed to sdd1, and so one... until sdf1... It is the first time i have the issue, it might be hardware, i sent the CPU back to Deltatau. Thanks again Kejr! Anthony Link to comment Share on other sites More sharing options...
lovu Posted November 27, 2020 Share Posted November 27, 2020 The device names of disk partitions are unstable; hardware reconfiguration, and adding or removing a device can cause changes in names. This is the reason why it's strongly recommended to use filesystem or partition identifiers like UUID or LABEL to indicate the device and filesystem. Link to comment Share on other sites More sharing options...
Recommended Posts